RSTLED is on

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
7,055件の閲覧回数
fahmirazak
Contributor II

hi guys..

want to ask..why my trkmpc560xb when connected to power supply, the RSTLED is on..it is broken or something..?

tq

1 解決策
6,568件の閲覧回数
DamarisOchoa
NXP Employee
NXP Employee

Hello fahmirazak

I hope  your issue got solved back in may. But if it didn´t, I asked around and the Reset Led is on when you press the reset button, normally. But in case you are not pressing the button, it means the micro is resetting itself. This could mean that there is a program doing it or that there is nothing on the flash. It could also be a problem with the microcontroller.

Depending if you can program you mcu, is if it is broken.

Regards,

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
6,568件の閲覧回数
DamarisOchoa
NXP Employee
NXP Employee

Hello fahmirazak

I hope  your issue got solved back in may. But if it didn´t, I asked around and the Reset Led is on when you press the reset button, normally. But in case you are not pressing the button, it means the micro is resetting itself. This could mean that there is a program doing it or that there is nothing on the flash. It could also be a problem with the microcontroller.

Depending if you can program you mcu, is if it is broken.

Regards,

0 件の賞賛
返信
6,568件の閲覧回数
rogercovarrubia
Contributor III

The same thing happens to me but once i flash it the led goes off, then when i plug it again to a source power tsomethimes the led goes on again, But it just happens on some programs that i flash i think (I hope) that it is a register that is corrupted or something

0 件の賞賛
返信
6,568件の閲覧回数
rogercovarrubia
Contributor III

Mine is a mpc5606b

0 件の賞賛
返信
6,568件の閲覧回数
FlavioStiffan
NXP Employee
NXP Employee

Can you flash it?

0 件の賞賛
返信
6,568件の閲覧回数
FlavioStiffan
NXP Employee
NXP Employee

murraystewart-b04629 do you have 2 min to check this out? maybe you have an answer to this.

Thanks

6,568件の閲覧回数
fahmirazak
Contributor II

cant flash..do you have any idea?

0 件の賞賛
返信