大学项目知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

University Programs Knowledge Base

讨论

排序依据:
Embedded processors are highly optimized products.  When you just want a good general use processor, sifting through the many options to find the best one can be daunting.  Below are some excellent general-purpose use platforms that I recommend for academia.  Are there other options, you bet.  These are the best in class, most popular and great for learning. FRDM-KL25Z TWR-K60D100M Wand Board Teensy 3.0 Cost: $12.95 $99 ($169 for -KIT) $79/$99/$129 $19 Chip: Cortex-M0+ Cortex-M4 Cortex-A9 (Single/Dual/Quad core) Cortex-M4 On-Board Features: Minimal Good Good Very Minimal Expansion Capability Excellent Good Average Good Notable Features Arduino Shield Compatibility Program with mbed.org I/O options Android Jellybean, HDMI Plug into breadboard Program with Arduino IDE The Freedom Board (FRDM-KL25Z) This is a great starter board!  It's cheap($12.95), yet powerful and can be used in a wide variety of applications.  All FRDM- boards are pinned out in the Arduino shield standard so you have lots of expansion options.  The FRDM-KL25Z can be programmed with the normal 'industrial strength' IDE you can also use mbed.org which sets it apart from many other products in this list for ease-of-use. Teensy (Teensy3) Made by PJRC.  For those that want to put a high performance 32-bit MCU on a breadboard.  Also, per the PJRC website you you are able to use the Arduino IDE.  The hardware is about as bare-bones as it gets, but the nice small footprint and breadboard ability gives you lots of flexibility to add your own custom I/O. The Tower System (TWR-K60D100M-KIT) The Tower System is another platform with a multitude of options.  With the Tower System you get access to much more I/O and is designed with higher performance applications in mind.  The particular variant I most often recommend is the TWR-K60D100M simply because it has so many features all packed in.  USB, Ethernet, Crypto engine, CAN, SPI, I2C and the list goes on.  Couple that with plenty of processing muscle with a Cortex-M4 CPU running at 100Mhz. Wand Board.org (Wand Board) The Cortex-M series is primarily intended for embedded control applications.  Whereas the Cortex-A series is built for graphical and multimedia applications.  Wandboard.org has been getting a lot of attention in the community as a Rasberry PI, Beagle Bone alternative(comparison chart).  Another similar product, still in development, is UDOO so stay tuned for that one.
查看全文
A great exercise when first starting with a new microcontroller is to get LEDs to turn-on, flash, or dim. Depending upon the configuration of your circuit, a LED (light-emitting diode) is accessed by toggling a GPIO or 'General Purpose Input Output pin either high or low. GPIO pins can be configured either as an input (read) or output (write). A high signal is often referred to as "Asserted" or a logic "1" and a low signal designated as Negated or logic "0". The input and output voltage range for GPIO pins is typically limited to the supply voltage of the evaluation board. Usage To optimize functionality in small packages, physical microcontroller pins have several functions available via signal multiplexing. Internally, a pin will have several wires connected to it via a multiplexer (wiki) or MUX. A multiplexer selects between several inputs and sends the selected signal to its output pin. The Signal Multiplexing chapter of your reference manual illustrates which device signals are multiplexed on which external pin. The Port Control block controls which signal is present on the external pin. The configuration registers within a microcontroller require proper configuration to select the GPIO as an input or output. The same GPIO pins utilized to blink a LED can be wired to read a signal coming from an external device such as the input from a hall effect sensor. Freescale Cup participants will configure GPIO pins as outputs to control the line-scan-camera via timed pulses and clock type signals. Read/Write In write mode, the GPIO pin can be set, cleared, or toggled via software initiated register settings. To determine which pin on the microcontroller is connected to a LED and how to access it from software, refer to the schematic of the microcontroller board. This pin will have numeric or alfanumeric value as well as an descriptive designation such as PTC7. Microcontroller Reference Manual: GPIO Information You will find high level information about GPIO usage in several different areas of a reference manual. See thereference-manual article for more general information. Relevant Chapters: Introduction: Human-machine interfaces - lists the memory map and register definitions for the GPIO System Modules: System Integration Modules (SIM) - provides system control and chip configuration registers Chip Configuration: Human-Machine interfaces (HMI). Signal Multiplexing: Port control and interrupts Human-Machine Interfaces: General purpose input/output Hardware As stated before, internal registers control whether a pin is high or low. Determining the polarity or orientation of your LED is important because this will let you know whether to set the associated pin in the HIGH or LOW state. The evaluation boards from Freescale all provide LED circuits like the one shown below. LED Circuit The circuit in figure (1) demonstrates a simple way to to power a LED. The circuit consists of connecting in a LED, resistor (which limits the current) and voltage source in series. LED's are semiconductors which convert current to light. When they are forward biased (turned on), electron and holes will recombine with no change in momentum, emitting a photon or light wave. Choosing the resistor is simple if you know the operating current requirements for your LED which are determined by reading the LED datasheet or specification document. R = (Vs - VL)/ IL Where V s is the power supply voltage, and V L is the Voltage Drop across the LED, and I L is the desired current through the LED.
查看全文
Sifting through technical documentation is part of an engineers job.  Sometimes these documents can be hundreds or thousands of pages long, so knowing where to makes life much easier.  This article is going to try to help you navigate smarter... Freescale has the following structure for technical documents: Reference Manuals (Usually end with "RM") - These are typically the thick manuals.  You will find sections detailing operation, registers, and electrical characteristics. Data Sheet (Usually ends with "DS") - These are quick summaries of the specifications of the device.  Includes electrical characteristics such as operating voltages, input and output minimum and maximum ranges.  In addition to environmental characteristics such as temperature ranges and graphs of performance vs. certain conditions. Schematic (_SCH) - This is typically referred in terms of board designs.  A schematic is useful in finding out how and where an external thing (LED, button, Display) is connected to the microcontroller.  Fact Sheet (_FS) - This is generally overview type information.  Useful when you are trying to determine which microcontroller you want to use.  Errata - Sometimes there are bugs in the chip.  When these are discovered the company issues an errata.  Sometimes the item get's fixed in the next revision of the chip, sometimes you just work around the problem.  If you think it should be working and it's not check the erratas! Tips and Tricks Use the search or find function all the time. Shortcut key '''(Ctrl-F).''' Use two monitors. Have the document open in one, search or browse to what you need to find and simply copy and paste the configuration information into your IDE. Search tips:  Use the pin name.  (I.e. PTC, PORTA, or FTM) Save trees only print out what you need. Commonly Used Acronyms: PDB - Programmable Delay Block FTM - Flex Timer Module ADC - Analog to Digital Converter DAC - Digital to Analog Converter MCG - Multipurpose Clock Generator SPI - Serial Programming Interface CnV - Channel n Value CNTIN - Counter Initial Value SIM - System Integration Module SIM_SCGCn - System Integration Module, System Clock Gating Control Register CMP - Comparator Module SIM - Provides system control and chip configuration registers. You will use this to turn on the clocks to particular peripherals. The SIM_SCGC
查看全文
GEORG is the Rescue Robot from the Freescale Robotics Lab of the Georg-Simon Ohm University of Applied Sciences of Nuremberg (Germany). During last week's, the student team led by Prof. Stefan May have attended the Worldwide RoboCup finals in Eindhoven (The Netherlands) and scored #12. Quite a good result for GEORG as it is it's first entry into the world finals. The Robotics team has been working since last year porting ROS (Robotic Operating System) to the Freescale i.MX platform to save space and power vs. an onboard PC. They are also working in developing distributed ROS computing systems using Freedom boards as modules. See GEORG's progress on the Robotics page of the university
查看全文
The attached final rules are valid for the 2014 Freescale Innovation Competition rules
查看全文
Notes: Will ask - Do you want to add the Remote System to your workspace? Click yes Build - select flash Plug in your K40 board to the usb (tower is not needed in this step) Click on debug as it will ask you which configuration you want to launch: Select the internal flash one. Bottom right you will see it "Launching with a little green light indicating that it is programming your board. After clicking debug as, you will enter the debug Eclipse "view" nothing will happen until you press "resume" Download the Zip file which is located: LED BLINK 96MHZ How to: Set up a debug: Program the FLASH Click on project in codewarrior projects menu There is noe issue with the Kinetis chips errata 2448. The code which is in our zip file already has these changes made, but if you download Kinetis example code from the official freescale site instead of using the wiki code - it may not work. Read more about the work - around here: here ++ Test to make sure everything is working properly CodeWarrior typically defaults to a "pause" setting when the debug is first started. To test wheter the code is working you will need to press "resume"
查看全文
The Freescale linescan camera is based upon the TSL1401CL sensor from TAOS Inc. Design Files Schematic & 3D Render (Courtesy of eli_hughes) Images (Lens removed) Freescale Linescan Camera Specifications 128-pixel linear image sensor (TSL1401CL) Focusable imaging lens 5-pin physical interface on PCB on .100" grid Simple three-pin MCU interface with analog pixel output Lens: 7.9mm focal length, f2.4 fixed aperture, manual focus, 12mm x 0.5mm thread Exposure Time: 267µS to 68mS Resolution: 128 pixels Built-In amplifier stage to improve white/black differentiation. The lense used on the board: Alaud Optical     8.0mm f.l. Lens w/IR filter = Part Num: AB0825C        M12x.05 Lens Holder = #9 or #10 Useful links AMS TSL1401 Product Page Line Scan Camera Use Freescale App Note: Line Scan Camera
查看全文
This tutorial is meant to introduce you to the use of a push button. It will give an explanation and example code of how you could implement a push button. Push buttons can be a great way to set a number of different states. Push buttons are advantageous because you can change your code physically versus pulling up the debugger every time you want to make a little change. ------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------ Usage A button can have many different functions on your autonomous vehicle. Most notably the button has been used for testing to start, stop, or put your car in a configuration mode. Configuration mode would let you test to see if all the peripherals except the motors are working. This would help you test your camera data and servo angles without always having to run after your car. During your race you can even set your button to different speed states. Since you have two chance to traverse the track you may have a slower safer speed on one state and a faster speed the pushes the limit on another state. In the end, what you do with the button is up to you and the choices are unlimited. Description of Example Code Below there will be an example of how to implement a push button. This push button will be connected to PTA16. When reading this pin a high, "1" or 5V, is considered "OFF" and a low, "0" or 0V, is considered "ON." To reduce the effects of bounce and/or the chance of a false press, additional code has been added to filter the signal. This is done by checking the button every 10ms for 50ms. If the button has been pressed for 3 or more of the 5 times we will change the state, otherwise it will not be considered a "press." Button Initialization Here is the initialization code that can be put in a header such as "Button.h." #define BUTTONLENGTH 5   // Button's Defined State   // 0 means button not pressed   // 1 means button pressed short fButton = 0; short iButtonCount=0; short iButtonTimer=0;   // Button Triggered Start time short iButtonTime; void initButton() {   //turn on clock to Port A   SIM_SCGC5 |= SIM_SCGC5_PORTA_MASK;   // configure pin to be GPIO   PORTA_PCR16 = PORT_PCR_MUX(1) | PORT_PCR_DSE_MASK;   // configure PTA16 to be input   GPIOA_PDDR &= (0<<16);  } See GPIO for explanation of how these specific commands work. Button Implementation Below is an example of a function that implements the button function. This function can be stored in a header file "Button.h" along with the initialization code. To call this function you would just place "readButton();" in your 10ms Flextimer source code. Read comments for description of each line Void readButton () {                  short fButtonState  = 0;   // initializes the button state to "OFF"           iButtonCount++;            // increments button count      if (GPIOA_PDIR & (1<<16)) {                    // if button read as high then its off otherwise its on           fButtonState = 0;      } else {           fButtonState = 1;      }      if (fButtonState && ! fButton) {                          // if the button is pushed and it previously wasn't then start a count           iButtonTimer++;           if (iButtonTimer <= 1) {                                                             iButtonCount = 0;                                 // Reset the Button Count if the timer is less or equal to 1           }      } else if (! fButtonState && fButton) {           iButtonTimer++;           if ( iButtonTimer <= 1) {                iButtonCount = 0;                               // Reset the Button count if the timer is less or equal to 1           }      }      if ( iButtonCount > BUTTONLENGTH && iButtonTimer >0) {     // if button has been read for 50ms check to see if we passed the test!           if ( iButtonTimer > (3*BUTTONLENGTH/4) && fButton) {                // fButton = 0;           } else if (iButtonTimer > (3*BUTTONLENGTH/4) && ! fButton) {                fButton = 1;           }           iButtonCount = 0;           iButtonTimer = 0;     } }
查看全文
Freescale - North America - is looking for you!  If you want to use the innovative and fresh ideas you are learning in the classroom to contribute to projects that help change lives, then a Freescale internship or co–op position is for you. I want to know more about Freescale internship and co-op opportunities. University Recruiting Calendar for 2013 Quick Facts about Freescale Freescale at a Glance Research More University Programs opportunities(PDF attachment)
查看全文
Congratulations to all the teams to making it this far.  Last minute tweaks made and broke a few teams shooting for the top spot. Best times: (in seconds) 14.89 - Beijing University of Science and Technology [China] 17.60 - Swinburne University of Technology [Malaysia] 19.08 - National Taiwan University of Science and Technology [Taiwan] 19.57 - Escola Politecnica da Universidade de Sao Paulo [Brazil] 20.54 - University of California Berkeley [USA] 22.14 - Slovak University of Technology [Slovakia] DNF - The University of Tokyo [Japan] DNF - Bannari Amman Institute of Technology [India] DNF - Instituto Politecnico Nacional [Mexico] Read more: Day 1: Freescale Cup 2013 Worldwide Championship and China Regional Finals Day 2:  (coming soon)
查看全文
Join Professor Richard Balogh and his students as they explain how they mastered the challenges of The Freescale Cup and won the 2013 EMEA title in March this year. The team FEI-Minetors from the Slovak Technical University in Bratislava also attended The Freescale Cup Worldwide Challenge held in Harbin, China this summer. To see our event schedule, join us on The Freescale Google+ page at https://www.google.com/+freescale
查看全文
This tutorial covers the specific details of obtaining data from the line scan camera on the Qorivva TRK-MPC5604B board. This tutorial will help students familiarize themselves with how to interface the camera with the microcontroller, how to configure GPIO pins to create clock signals and also how to utilize the microcontroller's ADC to read the data from the camera. Outside of control algorithms, configuring the camera is one of the more complex tasks necessary to create a Freescale Cup Vehicle. 1. Overview 2. Hardware 3. Set up the Hardware: Line Scan Camera/Microcontroller Hardware Setup 4. Build the Code 5. Download/Debug/Run 6. Learning Step Functions Calling the Function Variables Setting threshold. (This can give you a simple view of what your camera sees without connecting it to a scope) Sample Code Download Link Alternative Examples Other Qorivva Tutorials: Links External 1. Overview In this exercise students will access the line scan camera, create a clock signal and create the initialization pulse which tells the camera to begin the exposure period. This tutorial will not describe line recognition or line following algorithms - these concepts are beyond its scope. Students will: Open the example file using Codewarrior Build a project Download the code to the board connect the microcontroller to the camera via the motor control board Run the program view the camera data, clock and Si pulse on an oscilloscope To successfully complete this exercise, students will need the following board and development environment: TRK-MPC5604B Motor Drive Board Version A Freescale Cup TRK-MPC5604B compatible Car Kit CodeWarrior for Microcontrollers v 2.8 P&E Micro Toolkit Freescale Line Scan Camera USB Cord Knowledge of how Pointers and arrays are utilized in C 2. Hardware   Read the Obtain Data From Line Scan Camera overview article for general information on the camera, ADC, and GPIO microcontroller configuration settings. Connect the sensors, motor drive board and microcontroller of your car according to the TRK-MPC5604B chassis build instructions 3. Set up the Hardware: Line Scan Camera/Microcontroller Hardware Setup It is crucial for an engineer to have the proper test equipment and tools for the job. In this case, without an oscilloscope, students will not be able to verify whether the proper signals are being sent to the camera, or that the camera is working properly. 4. Build the Code If there is more than one project in your project view, make sure the proper project is the focus. The most reliable way to do this is to right click the project and choose Build Project as shown below. You can also go to the Project menu and choose the same command. If errors are encountered, look in the Problems view and resolve them. For now ignore any warnings. 5. Download/Debug/Run Download the code to your board, once this process is complete resume the project so that the code runs. 6. Learning Step What will happen: the function ImageCapture() is called in main.c with a pointer to the first element in the array. This function completes the processes necessary to capture images using the camera. To become more familiar with Pointers and Arrays - navigate to the C Programming Tutorial. Knowledge of Pointers and Arrays is a pre-requisite for understanding the Camera Code. Functions void CAMERA(void) {   TransmitData("****Line Sensor Test****\n\r");   SIU.PCR[27].R = 0x0200; /* Program the Sensor read start pin as output*/   SIU.PCR[29].R = 0x0200; /* Program the Sensor Clock pin as output*/   for(j=0;j<2;j++)   //for(;;)   {   SIU.PCR[27].R = 0x0200; /* Program the Sensor read start pin as output*/   SIU.PCR[29].R = 0x0200; /* Program the Sensor Clock pin as output*/   SIU.PGPDO[0].R &= ~0x00000014; /* All port line low */   SIU.PGPDO[0].R |= 0x00000010; /* Sensor read start High */   Delay();   SIU.PGPDO[0].R |= 0x00000004; /* Sensor Clock High */   Delay();   SIU.PGPDO[0].R &= ~0x00000010; /* Sensor read start Low */   Delay();   SIU.PGPDO[0].R &= ~0x00000004; /* Sensor Clock Low */   Delay();   for (i=0;i<128;i++)   {   Delay();   SIU.PGPDO[0].R |= 0x00000004; /* Sensor Clock High */   ADC.MCR.B.NSTART=1; /* Trigger normal conversions for ADC0 */   while (ADC.MCR.B.NSTART == 1) {};   adcdata = ADC.CDR[0].B.CDATA;   Delay();   SIU.PGPDO[0].R &= ~0x00000004; /* Sensor Clock Low */   Result[i] = (uint8_t)(adcdata >> 2);    }   Delaycamera();   //printlistall();   }   printlistall(); } Calling the Function within the main for loop in main.c, call the camera function using the following code: for (;;)   {   CAMERA();   } Variables Creates an 128x1 array for camera data information volatile uint8_t Result[128]; /* Read converstion result from ADC input ANS0 */   Setting threshold. (This can give you a simple view of what your camera sees without connecting it to a scope) #define THRESHOLD (2.0 /*volts*/ / 0.03125) // 8-bit A/D = 31.25mV/bit CAMERA(); // read line sensor, 128x1 pixel result returned in Result[128] array // print result for (i = 16; i < 112; ++i) // ignore the first and last 16 bits in the camera frame   if (Result[i] < THRESHOLD)   TransmitCharacter('1'); // black (low intensity)   else   TransmitCharacter('0'); // white (high intensity) Sample Code Download Link Qorivva Sample Code Download Link Alternative Examples Application Note 4244 and Software. Other Qorivva Tutorials: 1. Qorivva: Blink LED 2. Qorivva: Drive DC Motor Tutorial 3. Qorivva: Turning A Servo 4. Qorivva: Line Scan Camera Tutorial Links Qorivva Overview https://community.nxp.com/docs/DOC-1019 External TRK-MPC5064B Freescale Webpage TRK-MPC5064B Freescale Reference Manual TRK-MPC5064B Freescale Schematic
查看全文
MCU101 (Theory Topics)   Know Your Microcontrollers   Blink LED   Drive a DC Motor   Turn a Servo   https://community.nxp.com/docs/DOC-1030   Navigating Technical Documentation   C programming for Embedded System Software Tools CodeWarrior Software Development Tools & IDE CodeWarrior Beginners Tutorial (videos)   TRK-MPC 5604B Hardware Setup   Creating a new bareboard project   Debugging a bareboard project   Importing projects and merging code   Discussion of the header files (part 1)   Discussion of the header files (part 2) Qorivva Specific (with Code) Beginners Hands-on Tutorials Blink LED Drive DC Motor Turn A Servo Line Scan Camera Hardware https://community.nxp.com/docs/DOC-1016 DIY Camera Mounting Wiring Connections for TRK-MPC5604b Batteries Advanced Tutorial Series Push-Buttons   I2C Sensors using Kinetis K40 Miscellaneous Topics PCB design tips
查看全文
http://www.freescale.com - FTF on-the-street reporter talks to ITESM from Guadalajara, Mexico who describe their challenges and learnings in building an inte...
查看全文
ARM University Programs Lab-in-a-Box (LiB) Freescale and ARM University Programs have teamed up to provide you the Lab in a Box.  If you are interested in adopting the Lab-in-a-Box (LiB) in your course please contact the ARM University Program to request a donation! Development Boards The FRDM-KL25Z is an ultra-low-cost development platform enabled by Kinetis L Series KL1x and KL2x MCUs families built on ARM® Cortex™-M0+ processor. Features include easy access to MCU I/O, battery-ready, low-power operation, a standard-based form factor with expansion board options and a built-in debug interface for flash programming and run-control. The FRDM-KL25Z is supported by a range of Freescale and third-party development software. Freedom Development Platform Lab Exercise for Freescale Freedom KL25Z Board Software Tools ARM offers the Keil Microcontroller Development Kit (MDK-ARM) for ARM powered microcontrollers. It features the industry-standard compiler from ARM, the Keil µVision IDE, and sophisticated debug and data trace capabilities. MDK-ARM offers tailored support for all Cortex-M processor-based devices, and is the recommended solution for students working with standard ARM-based MCU devices. We suggest that students and universities download the free evaluation version of the tools, which offers all the features of the standard version, but with a 32 KByte object code/data limit. Keil Microcontroller Development Kit (MDK-ARM) Textbooks The Definitive Guide to the ARM Cortex-M0 In English, by Joseph Yiu Published by Newnes ISBN-10: 0123854776 ISBN-978-0123854773 C Programming for Embedded Microcontrollers In English, by Warwick A. Smith Published by Elektor ISBN: 978-0-905705-80-4Other ARM-related Books Teaching Materials Teaching Slides ARM Processors and Architectures Comprehensive Overiew - 2012 ARM Processors and Architectures Fundamentals Lab Manuals and Exercises Lab Exercises for Cortex-M4 Freescale Kinetis using Keil MDK Lab Exercises for Cortex-M0+ Freescale Freedom KL25Z Board Application Notes for Students and Faculty AN234: Migrating from PIC Microcontrollers to Cortex-M Other Projects and Resources Variety of Resources and Middleware from onARM Projects-Lab.com - Ideas for Design Projects Other ARM Projects
查看全文
1. Download CodeWarrior 2.8 Evaluation Version (Classic, Windows-hosted) To Program your microcontroller you will need to set up the CodeWarrior Integrated Development Environment. CodeWarrior is available on the Freescale.com Website. Method 1: Direct Link direct download link (Caution - link may not be up to date) Method 2: Navigate to the Download Link From Freescale.com click on: "Design Resources" tab at the top of the page, then navigate to "Software and Tools", and then to "Codewarrior Devleopment Tools" Click on the "Download CodeWarrior now link" Click on the Download Evaluation Versions link" Within this page, use your browser "find" feature (Typically CTRL-F) to search for the text string "V2.8" Click the "download" button next to "Evaluation: CodeWarrior for MPC55xx/MPC56xx Microcontrollers V2.8 (Classic)". and save it to your computer. 2. Install CodeWarrior To install CodeWarrior Development Studio for Microcontrollers v2.8, double-click the installation package and a wizard will guide you through the installation process. Installation Notes: Are you using Windows Vista or Windows 7? Evaluation Edition User: If you are installing the Evaluation Edition, the Evaluation license is automatically installed with your product and you do not need to register it. This license allows you to develop projects as Professional Edition within the 30-day evaluation period. After 30 days, the license works as Special Edition license (free permanent, but feature limited) which supports unlimited assembly code, up to 32KB of C code for HCS08/RS08 derivatives, up to 64KB of C code for V1 ColdFire derivatives and up to 128KB of C code for V2-V4 ColdFire and Kinetis derivatives and up to 512KB of C code for MPC56xx derivatives. Once you have finished downloading and installing CodeWarrior, users can return to Downloading and Installing P&E as part of the Blink a LED on Qorivva Tutorial
查看全文
2013 Global Freescale Cup Champion. Video Link : 1589 Car Specs: Custom K60 Control Board
查看全文
Here are some special offers from our partners from around the world: MathWorks support software for The Freescale Cup participants Stay tuned... more to come
查看全文
Freescale india and CEDT, IISc organised Freescale Cup - Smart car race india 2011 Final Run of Grand Prize(Rs. 1,00,000) winner team from NIT,Surat. Student... Amit Tank, Atit JAriwala, Vivek Kholia, Suraj Das
查看全文