ユニバーシティ・プログラムのナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

University Programs Knowledge Base

ディスカッション

ソート順:
Find the complete material at: https://community.freescale.com/docs/DOC-95205
記事全体を表示
Find complete materials at: https://community.freescale.com/docs/DOC-95205
記事全体を表示
Find complete material at: https://community.freescale.com/docs/DOC-95205
記事全体を表示
Find the complete material at https://community.freescale.com/docs/DOC-95205
記事全体を表示
Find complete materials at https://community.freescale.com/docs/DOC-95205
記事全体を表示
Find the complete material at:https://community.freescale.com/docs/DOC-95205
記事全体を表示
Find the complete material at: https://community.freescale.com/docs/DOC-95205
記事全体を表示
Find the complete material at: https://community.freescale.com/docs/DOC-95205
記事全体を表示
Using Header(.h) files provided by Freescale inside CodeWarrior - Blinking an LED
記事全体を表示
Examines the core used in the MKL25Z128VLK4 device that is mounted on the FRDM-KL25Z board. The audience will be guided through the process of acquiring documentation for both the device and the core. A brief overview of the ARM cortex series will be presentated and how it relates to the embedded systems landscape.
記事全体を表示
This tutorial covers the details of Turning A Servo on the Kinetis K40 using TWR-K40x256-KIT evaluation board. Overview In this exercise you will build a “bare metal” (no RTOS) application which turns a servo, targeting a Freescale K40 board. You will: Create the Servo code in CodeWarrior Build the Servo project Download and run the code on a Kinetis K40 Tower System board Learn how to utilize the FlexTimer module to control a Servo   To successfully complete this exercise you need the following board and development environment. The K40 Tower card, TWR-K40x256 Tower Elevator Panels Servo Prototyping Board Power to your servo - either utilize the 7.2v Nicad Battery or a DC power supply CodeWarrior for Microcontrollers 1. Hardware 2. Create a New CodeWarrior Project 3. Build the Code 4. Download/Debug/Run 5. Learning Step: Servo Code Description Example Code Variables Init_PWM_Servo PWM_Servo PWM_Servo_Angle Set Up a Look-Up Table for Servo Angles Other K40 Tutorials: Links 1. Hardware   The first step of this tutorial requires you read the Turn A Servo article for background information on servo's, timer modules, PWM signals and counters. You will need to connect your servo to the microcontroller and also to a separate power source. 2. Create a New CodeWarrior Project The next step is to create a new project (or add this code to an existing project). 3. Build the Code If you have more than one project in your project view, make sure the proper project is the focus. The most reliable way to do this is to right click the project and choose Build Project as shown below. You can also go to the Project menu and choose the same command. If you encounter errors, look in the Problems view and resolve them. You can ignore any warnings. 4. Download/Debug/Run This link shows a video of the servo turning the wheels from left to right in small increments http://www.youtube.com/watch?v=QgwASk9DHvU&feature=relmfu 5. Learning Step: Servo Code Description Your code will sweep your servo from max to minimum angular position, and then back again continuously. Example Code This code sets up the Pulse Width Modulation Timer Module for use by a servo. It is set to utilize Edge-Aligned PWM, and this file properly configures the period, and pulse width for use by the other modules Several important functions are contained in this file: 1. Init_PWM_Servo () - initializes the timer module 2. PWM_Servo (double duty_Cycle) - enter the desired duty cycle setting for the servo 3. PWM_Servo_Angle (int Angle) - enter the desired angle for the servo Straight forward - PWM_Servo_Angle (45) Full left - PWM_Servo_Angle (90)Full right - PWM_Servo_Angle (0)   4. Servo_Tick - interrupt routine which executes once/servo period PWM_Servo (double duty_Cycle) Init_PWM_Servo () PWM_Servo_Angle (float Angle) void ServoTick() Variables FTM0_CLK_PRESCALE TM0_OVERFLOW_FREQUENCY Pulse_Width_Low Pulse_Width_High Total_Count Low_Count Scale_Factor Angle Init_PWM_Servo Void Init_PWM_Servo () { //Enable the Clock to the FTM0 Module SIM_SCGC6 |= SIM_SCGC6_FTM0_MASK;  //Pin control Register (MUX allowing user to route the desired signal to the pin.  PORTC_PCR4  = PORT_PCR_MUX(4)  | PORT_PCR_DSE_MASK; //FTM0_MODE[WPDIS] = 1; //Disable Write Protection - enables changes to QUADEN, DECAPEN, etc.  FTM0_MODE |= FTM_MODE_WPDIS_MASK; //FTMEN is bit 0, need to set to zero so DECAPEN can be set to 0 FTM0_MODE &= ~1; //Set Edge Aligned PWM FTM0_QDCTRL &=~FTM_QDCTRL_QUADEN_MASK;  //QUADEN is Bit 1, Set Quadrature Decoder Mode (QUADEN) Enable to 0,   (disabled) // Also need to setup the FTM0C0SC channel control register FTM0_CNT = 0x0; //FTM Counter Value - reset counter to zero FTM0_MOD = (PERIPHERAL_BUS_CLOCK/(1<<FTM0_CLK_PRESCALE))/FTM0_OVERFLOW_FREQUENCY ;  // Count value of full duty cycle FTM0_CNTIN = 0; //Set the Counter Initial Value to 0 // FTMx_CnSC - contains the channel-interrupt status flag control bits FTM0_C3SC |= FTM_CnSC_ELSB_MASK; //Edge or level select FTM0_C3SC &= ~FTM_CnSC_ELSA_MASK; //Edge or level Select FTM0_C3SC |= FTM_CnSC_MSB_MASK; //Channel Mode select //Edit registers when no clock is fed to timer so the MOD value, gets pushed in immediately FTM0_SC = 0; //Make sure its Off! //FTMx_CnV contains the captured FTM counter value, this value determines the pulse width FTM0_C3V = FTM0_MOD; //Status and Control bits FTM0_SC =  FTM_SC_CLKS(1); // Selects Clock source to be "system clock" or (01) //sets pre-scale value see details below FTM0_SC |= FTM_SC_PS(FTM0_CLK_PRESCALE); /******begin FTM_SC_PS details **************************** * Sets the Prescale value for the Flex Timer Module which divides the * Peripheral bus clock -> 48Mhz by the set amount * Peripheral bus clock set up in clock.h *  * The value of the prescaler is selected by the PS[2:0] bits.  * (FTMx_SC field bits 0-2 are Prescale bits -  set above in FTM_SC Setting) *  *  000 - 0 - No divide *  001 - 1 - Divide by 2 *  010 - 2 - Divide by 4 *  011 - 3 - Divide by 8 *  100 - 4 - Divide by 16 *  101 - 5 - Divide by 32 *  110 - 6 - Divide by 64 - *  111 - 7 - Divide by 128 *  ******end FTM_SC_PS details*****************************/ // Interrupts FTM0_SC |= FTM_SC_TOIE_MASK; //Enable the interrupt mask.  timer overflow interrupt.. enables interrupt signal to come out of the module itself...  (have to enable 2x, one in the peripheral and once in the NVIC enable_irq(62);  // Set NVIC location, but you still have to change/check NVIC file sysinit.c under Project Settings Folder } PWM_Servo Void PWM_Servo (double duty_Cycle) {          FTM0_C3V =  FTM0_MOD*(duty_Cycle*.01); } PWM_Servo_Angle //PWM_Servo_Angle is an integer value between 0 and 90 //where 0 sets servo to full right, 45 sets servo to middle, 90 sets servo to full left void PWM_Servo_Angle (float Angle) {    High_Count = FTM0_MOD*(Pulse_Width_High)*FTM0_OVERFLOW_FREQUENCY;    Low_Count = FTM0_MOD*(Pulse_Width_Low)*FTM0_OVERFLOW_FREQUENCY;    Total_Count = High_Count - Low_Count;    Scale_Factor = High_Count -Total_Count*(Angle/90);     FTM0_C3V = Scale_Factor; //sets count to scaled value based on above calculations } Set Up a Look-Up Table for Servo Angles int main(void) {   //Servo angles can be stored in a look-up table for steering the car.   float table[n] = { steering_angle_0;    steering_angle_1;    steering_angle_2;   ……    steering_angle_n-1    };   Steering_Angle = table[x];   PWM_Servo_Angle (Steering_Angle); // Call PWM_Servo_Angle function. } Other K40 Tutorials: K40 Blink LED Tutorial K40 DC Motor Tutorial Kinetis K40: Turning A Servo K40 Line Scan Camera Tutorial Links Kinetis K40 TWR-K40X256-KIT
記事全体を表示
DIP breakout board for the Kinetis Microcontrollers   2 layer board of 0.65x1.35 inches (16.54x34.29 mm).  Minimal component requirements. You can buy the board from Osh Park ($4.95) or download the design files here! Thanks dgd for sharing the link!
記事全体を表示
This guide provides all the participants of the Freescale Cup finals with the key information to get organised during the event. This is the final version
記事全体を表示
What is a microcontroller (MCU)? A microcontroller includes a microprocessor (CPU) as well as a number of other components like RAM, flash and EEPROM to store your programs and constants. While a microprocessor requires external devices to control things like input/output, or timers to implement periodic tasks, and digital to analog converters, a microcontroller is all inclusive. Contrast this all-in-one approach with a typical personal computer which contains an INTEL or AMD CPU, as well as separate chips for RAM, a separate video card, a dedicated hard drive, silicon chips or PCI circuit boards to enable the processor to access USB, serial and video card signals Microcontroller pins are general purpose, whereas CPU pins are specific. This means that each pin is tied to a multiplexer which you must set to choose the particular use for the pin. For example, in a microcontroller, one pin pin might be re-purposed for the following tasks 1. The output of a timer 2. Send a signal to a motor 3. Receive an input from a sensor or analog device
記事全体を表示
This tutorial will introduce you to I 2 C and provide a framework that you can use to start communicating with various devices that use I 2 C. This tutorial is meant for the Kinetis K40 and will probably not work on any other Kinetis chip. DISCLAIMER: This has not been fully tested and may not work for you and for all devices. The header file provided does not handle errors and should not be used for critical projects. 2C signaling I2C header file Example of I2C communication using Freescale MMA8452Q 3-axis accelerometer Introduction to I 2 C signaling I 2 C is a simple two wire communication system used to connect various devices together, such as Sensory devices and microprocessors using 8 bit packets. I 2 C requires two wires: the first is called SDA and is used for transferring data, the second is called SCL and it is the clock used to drive the data to and from devices. I 2 C uses an open drain design which requires a pull up resistor to logic voltage (1.8,3.3,5) on both SDA and SCL for proper operation. I 2 C is a master-slave system where the master drives the clock and initiates communication. The I 2 C protocol has 5 parts. The Start signal which is defined as pulling the SDA line low followed by pulling SCL low. The slave device address including the Read/Write bit The register address that you will be writing to/ reading from the data The acknowledgement signal which is sent from the receiving device after 8 bits of data has been transferred successfully. the Stop signal, which is defined by SDA going high before SCL goes high. 1. The start signal is sent from the Master to intiate communication on the bus. The start and stop signals are the only time that SDA can change out of sync with SCL. Once the start signal is sent no other device can talk on the bus until the stop signal is sent. If for whatever reason another device tries to talk on the bus then there will be an error and the K40 can detect this. 2. The slave device is a 7 bit (sometimes 10bit but this will not be covered in this tutorial) address provided by the device and is specific to the device. The type of data operation (read/write) is determined by the 8 th bit. A 1 will represent a write and a 0 a read operation. 3. The register addresses are provided by the device's specifications. 4. The data you will send to a device if you are writing or the data that you receive from the device when reading. This will always be 8 bits. 5. After 8 bits of data has been transferred successfully the receiving device will pull the SDA line low to signify that it received the data. If the transmitting device does not detect an acknowledgement then there will be an error. The K40 will be able to detect this. 6. The stop signal is sent from the Master to terminate communication on the bus. Some devices require this signal to operate properly but it is required if there will be more than one master on the bus (which will not be covered in this tutorial) I2C header file This header file only has functions for reading and writing one byte at a time. Most devices support reading and writing more than one byte at a time without sending the Stop signal. Typically the device will keep incrementing the register's address to the next one during read/writes when there is no stop signal present. See your device's user manual for more information. /* * i2c.h * * Created on: Apr 5, 2012 * Author: Ian Kellogg  * Credits: Freescale for K40-I2C example */  #ifndef I2C_H_  #define I2C_H_  #include "derivative.h"  #define i2c_EnableAck() I2C1_C1 &= ~I2C_C1_TXAK_MASK #define i2c_DisableAck() I2C1_C1 |= I2C_C1_TXAK_MASK  #define i2c_RepeatedStart() I2C1_C1 |= I2C_C1_RSTA_MASK  #define i2c_Start() I2C1_C1 |= I2C_C1_TX_MASK;\    I2C1_C1 |= I2C_C1_MST_MASK  #define i2c_Stop() I2C1_C1 &= ~I2C_C1_MST_MASK;\    I2C1_C1 &= ~I2C_C1_TX_MASK  #define i2c_EnterRxMode() I2C1_C1 &= ~I2C_C1_TX_MASK;\    I2C1_C1 |= I2C_C1_TXAK_MASK  #define i2c_write_byte(data) I2C1_D = data  #define i2c_read_byte() I2C1_D  #define MWSR 0x00 /* Master write */  #define MRSW 0x01 /* Master read */  /* * Name: init_I2C * Requires: nothing * Returns: nothing * Description: Initalizes I2C and Port E for I2C1 as well as sets the I2C bus clock */  void init_I2C()  {    SIM_SCGC4 |= SIM_SCGC4_I2C1_MASK; //Turn on clock to I2C1 module    SIM_SCGC5 |= SIM_SCGC5_PORTE_MASK; // turn on Port E which is used for I2C1    /* Configure GPIO for I2C1 function */    PORTE_PCR1 = PORT_PCR_MUX(6) | PORT_PCR_DSE_MASK;    PORTE_PCR0 = PORT_PCR_MUX(6) | PORT_PCR_DSE_MASK;    I2C1_F = 0xEF; /* set MULT and ICR This is roughly 10khz See manual for different settings*/    I2C1_C1 |= I2C_C1_IICEN_MASK; /* enable interrupt for timing signals*/  }  /* * Name: i2c_Wait * Requires: nothing * Returns: boolean, 1 if acknowledgement was received and 0 elsewise  * Description: waits until 8 bits of data has been transmitted or recieved */  short i2c_Wait() {    while((I2C1_S & I2C_S_IICIF_MASK)==0) {    }     // Clear the interrupt flag    I2C1_S |= I2C_S_IICIF_MASK;  }  /* * Name: I2C_WriteRegister * Requires: Device Address, Device Register address, Data for register * Returns: nothing * Description: Writes the data to the device's register */  void I2C_WriteRegister (unsigned char u8Address, unsigned char u8Register, unsigned char u8Data) {    /* shift ID in right position */    u8Address = (u8Address << 1)| MWSR;    /* send start signal */    i2c_Start();    /* send ID with W/R bit */    i2c_write_byte(u8Address);    i2c_Wait();    // write the register address    i2c_write_byte(u8Register);    i2c_Wait();    // write the data to the register    i2c_write_byte(u8Data);    i2c_Wait();    i2c_Stop();  }  /* * Name: I2C_ReadRegister_uc * Requires: Device Address, Device Register address * Returns: unsigned char 8 bit data received from device * Description: Reads 8 bits of data from device register and returns it */  unsigned char I2C_ReadRegister_uc (unsigned char u8Address, unsigned char u8Register ){    unsigned char u8Data;    unsigned char u8AddressW, u8AddressR;    /* shift ID in right possition */    u8AddressW = (u8Address << 1) | MWSR; // Write Address    u8AddressR = (u8Address << 1) | MRSW; // Read Address    /* send start signal */    i2c_Start();    /* send ID with Write bit */    i2c_write_byte(u8AddressW);    i2c_Wait();    // send Register address    i2c_write_byte(u8Register);    i2c_Wait();    // send repeated start to switch to read mode    i2c_RepeatedStart();    // re send device address with read bit    i2c_write_byte(u8AddressR);    i2c_Wait();    // set K40 in read mode    i2c_EnterRxMode();    u8Data = i2c_read_byte();    // send stop signal so we only read 8 bits    i2c_Stop();    return u8Data;  }  /* * Name: I2C_ReadRegister * Requires: Device Address, Device Register address, Pointer for returned data * Returns: nothing * Description: Reads device register and puts it in pointer's variable */  void I2C_ReadRegister (unsigned char u8Address, unsigned char u8Register, unsigned char *u8Data ){    /* shift ID in right possition */    u8Address = (u8Address << 1) | MWSR; // write address    u8Address = (u8Address << 1) | MRSW; // read address    /* send start signal */    i2c_Start();    /* send ID with W bit */    i2c_write_byte(u8Address);    i2c_Wait();    // send device register    i2c_write_byte(u8Register);    i2c_Wait();    // repeated start for read mode    i2c_RepeatedStart();    // resend device address for reading    i2c_write_byte(u8Address);    i2c_Wait();    // put K40 in read mode    i2c_EnterRxMode();    // clear data register for reading    *u8Data = i2c_read_byte();    i2c_Wait();    // send stop signal so we only read 8 bits    i2c_Stop();    }  #endif  Example of I2C communication using Freescale MMA8452Q 3-axis accelerometer This example is very simplistic and will do nothing more than read the WHO AM I register to make sure that I 2 C is working correctly. To see more check out the Freescale MMA8452Q Example /* Main. C */ #include <stdio.h> #include "derivative.h" /* include peripheral declarations */ #include "i2c.h" int main(void) {      // checking the WHO AM I register is a great way to test if communication is working      // The MMA8452Q has a selectable address which is either 0X1D or 0X1C depending on the SA0 pin      // For the MMA8452Q The WHO AM I register should always return 0X2A      if (I2C_ReadRegister_uc (0x1D,0x0D) != 0x2A {           printf ("Device was not found\n");      } else {           printf ("Device was found! \n");      } }
記事全体を表示
Video Highlights of 2012 Competition Photographs from the Freescale Cup Japan 2012 competition.
記事全体を表示
This tutorial will discuss Timer Peripheral Modules, DC Motors, motor controllers, and configuration of your chip to output a PWM or Pulse Width Modulated Signal. The first section of this this tutorial provides the basics of DC (Direct Current) motors. The electronic circuits created to control these motors and schematics for PCBs, tips to reduce noise over important signals are also contained within this tutorial. Usage A dc-motor is an electrical device that converts energy into rotational movement. The motor moves a gear in one direction if current flows through the terminals (clockwise or counterclockwise), and in the opposite direction if current flows backwards through the same terminals. If there is a force opposing the motor, then the terminals are short circuited and the current through the terminals can go as high as 14 A or more. The voltage or current that must be delivered to the motor to work is too much for a microcontroller output port so an intermediary device must be used, such as the mc33932evb motor control board. Pulse Width Modulation (PWM) For a refresher in Pulse Width Modulation. Once you feel comfortable that you understand the concepts behind a duty cycle signal, you may move to the next step of understanding H bridge circuits. Circuit Amplification A microcontroller is typically not designed to directly drive DC motors.  Keep in mind MCU's are low-power devices and motors usually draw a lot of power.  So what is one to do?  Amplification!  There are lots of ways to do this and each has it's trade-offs.  Below are the most popular... Discrete Components A few MOSFETSs should do the trick.  This is a great learning exercise, you can probably get more oomph out of your circuit but it takes time to build and troubleshoot. If you search the web for motor driver board, you should find plenty of resources, designs, etc. Half-Bridge (aka H-bridge) These are integrated circuits with the aforementioned discrete components already configured for you.  Because these are integrated (into a very small footprint) these tend to be  power limited due to thermal issues.  Generally speaking, the better a device is at dissipating heat the more power it can handle. Get a basic view of H bridge circuit. Click here which describes H bridge circuits. DC Motor Describes how a DC motor works: here Microcontroller Reference Manual: Timer Information You will find high level information about Timer usage in several different areas of a reference manual. See the reference-manual article for more specific information on how best to navigate through to the areas which are relevant. Relevant Timer Chapters: Introduction: Human-machine interfaces - lists the memory map and register definitions for the GPIO System Modules: System Integration Modules (SIM) - provides system control and chip configuration registers Chip Configuration: Human-Machine interfaces (HMI). Signal Multiplexing: Port control and interrupts Human-Machine Interfaces: General purpose input/output Hardware Motor cup-car-motor: In testing the motor, we found that it drew between 0.35A and 0.5A with no load on the wheels and peaked at a little over 14A at stall. With this Data and 150% value for the H-Bridge or Motor Controller we need one with a current rating of 20A at least. The Motor has a Resistance between 0.9 and 1.0 ohm.  For motor control you can use the Freescale H-Bridge such as MC33931or MC33932, however these controllers peak at ~5 amps, so you will not be able to maximize speed Power & Current Requirements Additional Theory Training Resources Freescale Motor Control Tutorial Freescale Lecture 1: Introduction and Motor Basics Freescale Lecture 2: Pulse Width Modulaiton Freescale Lecture 3: Control Design Freesacle Lecture 4: Speed and Position Freescale Lecture 5: MPC5607B Overview
記事全体を表示
GEORG is the Rescue Robot from the Freescale Robotics Lab of the Georg-Simon Ohm University of Applied Sciences of Nuremberg (Germany). During last week's, the student team led by Prof. Stefan May have attended the Worldwide RoboCup finals in Eindhoven (The Netherlands) and scored #12. Quite a good result for GEORG as it is it's first entry into the world finals. The Robotics team has been working since last year porting ROS (Robotic Operating System) to the Freescale i.MX platform to save space and power vs. an onboard PC. They are also working in developing distributed ROS computing systems using Freedom boards as modules. See GEORG's progress on the Robotics page of the university
記事全体を表示
Freescale - North America - is looking for you!  If you want to use the innovative and fresh ideas you are learning in the classroom to contribute to projects that help change lives, then a Freescale internship or co–op position is for you. I want to know more about Freescale internship and co-op opportunities. University Recruiting Calendar for 2013 Quick Facts about Freescale Freescale at a Glance Research More University Programs opportunities(PDF attachment)
記事全体を表示