ユニバーシティ・プログラムのナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

University Programs Knowledge Base

ディスカッション

ソート順:
CW_MERGE_PROJECTS.wmv
記事全体を表示
2013 Global Freescale Cup Participant: Malaysia Car Specs: -Freescale Freedom FRDM-KL25Z
記事全体を表示
We are thrilled to present to you, the newest member of our Apalis family of ARM powered computer-on-modules, the Apalis iMX6. The module is based on Freescale i.MX 6 series of System-on-Chip (SoC), runs an ARM Cortex-A9 CPU, and offers an operating frequency of up to 1.2 GHz. Apart from the benefits of long term product availability (of more than 10 years), and compatibility with the existing Apalis T30 module, this module is also qualified for industrial temperature range -40° C to 85° C. More details including datasheet shall be published by the last week of February. For a preliminary datasheet, click here. For more details on Apalis family, click here. To know more about the Apalis T30 module, click here. Here's a first look at the module.
記事全体を表示
To comply with the rule that mentions that “One processor - No auxiliary processor or other programmable device is allowed”. Participants must check the camera used for the competition. The camera cannot have a processing unit that processes the image for localization, polarization, auto contrast or auto focus. The only authorization is for a compression engine (no image processing, only compression). An Analog to Digital external converter can be used. Such as AD7276/AD7277/AD7278. For any additional cameras, please contact your Regional Freescale Cup Coordinator. They can confirm if the camera can be used and it will be added to this list for further inquiries. Camera Allowed: TSL1401R−LF TSL1401-DB SEN-11745 OV-5116N Melexis MLX75306 Linear Optical Array Some restricted cameras and some examples why: OV-2540 This camera can be programmed and processes the image output. Not allowed. CM-26N/P This camera has • Auto gain, • Auto contrast and • Auto focused. OV6630 C3038 VGA OV7670
記事全体を表示
Lecture 1: Introduction and Motor Basics  This training module presented by Professor L. Umanand of CEDT, Indian Institute of Science, Bangalore provides an overview of the Freescale Cup – 2011. It introduces to the challenge describing the various components of the intelligent car tracker. Lecture 2: Pulse Width Modulation  This lecture provides an overview of Pulse Width Modulation Lecture 3: Control Design  This lecture describes controller design and PID control Lecture 4: Speed and Position  This Lecture discusses integrating your PID with sensor data Lecture 5: MPC5607B Overview  This training module provides an overview of the 32-bit Qorivva MPC5607B Processor. The course is targeted towards beginners in order to enable them to quick start the development of software on the MPC5607B.
記事全体を表示
Depending on which MCU Devlopment board you have chosen, you will need to figure out a way to mount this to the chassis. I have seen everything from cardboard, to aluminum, to wood. Below is a template complete with CAD drawings to mount the Qorivva TRK-MPC5604B board and the Motor Board onto the chassis. We use plexiglass for ours, but any other millable material is appropriate. The large hole in the middle is for cables from the servo. We attach the board to the car using the plastic standoffs (you will need them 55 mm long, so in our case, we used the combination of 40 + 15 mm) - see an example (SOS code 10260). To attach both the processor and interface boards the simillar 5mm plastic standoffs were used. Preview (.pdf) CAD file (.dxf)
記事全体を表示
Features General Tower card Form Factor Connections to allow use with a TRK-MPC5604B Board Camera Interfaces 1. 5-pin header to connect directly to Freescale Line Scan Camera 2. Header for 2nd linescan camera (optional) 3. RCA Camera Interface. Includes an LMH1981 Sync Extraction chip and connectors to MCU to allow for low resolution (32x32) decoding of signals Servo Outputs 3-pin Header to connector directly to steering Servo 1 Extra Servo header. Power Accepts direct Battery Power – Onboard Switching regulator 5-18v Tower Card will source power to other tower modules. All circuitry except for motor controller can be optionally powered over USB Connector Battery Input and motor Outputs will be a Tyco (TE Connectivity) TE Connectivity Screw Terminal http://search.digikey.com/us/en/products/1776275-2/A98036-ND/1826899 Motor Driver 2x MC33887APVW : Dual, Independent 5A Motor Driving Circuit Supports forward, reverse and braking. Current Feedback to MCU ADC to allow for closed loop torque control Programming Integrated Kinetis MK20DN512ZVLL10MCU with OSJTAG Can be used stand-alone or be used as a peripheral in the tower system. Additional I/O Extra signals from K40 routed to tower edge card connector. Signals for H-bridge, camera and servo can be routed to Tower Edge connector to be driven by another MCU card. Each can be disconnected via jumper. - We will need to crosscheck the signals to all other CPU modules. Would it be easier to just have a version that doesn't have the K40 populated and OSJTAG populated? Also, we may not need jumpers. Simply configure the Kinets I/O to inputs. Some basic I/O for debugging. 4-poistion DIP Switch + 4 LEDs. Inputs for Tach Signal/Speed Sensor Design Files Rev Alpha Schematics (Sent to MyRO on 4.4.2012) - Includes 3d view Assembly Prints (For Reference) PCB Fabrication Notes Bill of Materials Rev A Errata: Pins 4 & 5 for the camera (Gnd and +3.3v) got swapped on the PCB. You will need to swap the wires in the cable. You can pop the contacts out of the connector housing with tweezers. POT0 has a jumper wire to pin 26 (ADC1_SE18 . This was done to put all signals *except* the NTSC video onto ADC1 to simplify software. Future versions will have this change in the artwork Some components interfere with the tower connector. It can be mated to about 95%. Will work fine. Future versions will fix this issue Rev Beta Schematics, Assembly Prints, BOM, etc. - Includes 3d view Rev B Errata: None known! Google Code repository for the Example Code: https://code.google.com/p/tfc-twr/ This code works with Rev B of the board (and Rev A). All major interfaces & peripherals have been tested. At some point we will make a video going through the code. By default the Linescan camera code is enabled. The code in Main.c is pretty easy to follow. There is also code for the NTSC camera but must enabled in the TFC_Config.h file via a pre-processor directive. There is also code used for teh OSTAG interface, Labview demo applications and drivers for the USB Pictures Just verified the OSJTAG. Test Project to blink the battery LED's was downloaded into the K20 Videos Testing the Servo circuits….. Testing the pots, servos, H-bridges and K20 USB port Linescan Camera Bringup with Labview NTSC Camera Bringup with Labview 1.) This is a basic demo of an NTSC camera being brought in using the a Combo of the ADC, port interrupts and DMA transfers. 2.) I *ahem* overclock the ADC to 24MHz to get some extra resolution for a 64x64 pixel image (the first 6 columns are junk as they contain color burst data*) 3.) I decimate the images to a few frames per second to send over the WIFI (the booster pack card I made) to a Labview program. The Kinetis can bring the data in a the same frame rate of the camera, I just need to send much slower as there is some overhead in my communications scheme (ASCII text) and the WIFI is driven via a UART. 4.) In reality, I can get a 64 x 480 pixel image in memory as I pull in all the lines. I just decimate the rows to get a 64x64 result on the labview display. 5.) DMA does most of the work freeing up the CPU to do algorithms in the foreground.
記事全体を表示
First and foremost, be creative!! Below are just a few inspirational ideas. Option #1 - I cut-down (miter saw) a 4-position TWR-ELEVATOR to make this 2-position design. With the intent of having two boards mounted 1) TWR-PROTO and 2) MCU of choice (K40). If cutting PCB's with power tools is not your thing, you can buy a 2-position Tower Elevator here: http://wavenumber.net/twr-elev-2/ I just marked the holes on the back supportand drilled holes into the TWR-PROTO, a few stand-offs and viola! Option #2 - This option requires the removal of the rear spring. I am not sure how much value that spring honestly provides since most of the track is nice and flat. If you have a newer TWR-ELEVATOR you usually find some way to mount it to the screw holes with some form of L-Bracket. If you have an older TWR-ELEVATOR you can drill a hole in the Secondary Elevator (less PCB traces to worry about) and then mount it to the chassis with a L-Bracket. Option #3 - Check out this gallery of images: https://plus.google.com/u/0/photos/106056936857240793028/albums/5598207628299505201
記事全体を表示
Getting Started with the Freescale Cup How to achieve the goal of creating an autonomous vehicle that quickly navigates around a track? Before continuing with this tutorial, students should take the time to choose which Freescale Microcontroller your team is going to use. The Introduction to Freescale Cup Training article has some details about how to choose your microcontroller. Although the concepts and end results are similar no matter which microcontroller you decide to utilize, much of the software implementation details will differ. What is a Microcontroller? For information on what a microcontroller is head to the microcontrollers article. Getting Started - Learn to Program a microcontroller First off, you are going to need to know C programming. For a crash-course head to c-programming-for-embedded-systems. The classic first application to learn how to program a microcontroller is to get through the process of Blinking an LED. This wiki contains a tutorial for each of the Cup microprocessors which simplifies the process of setting up the evaluation board, installing the Integrated Development Environment, and programming the board with a simple set of software which blinks a LED. The Blink a LED tutorial is the first of 4 tutorials designed to familiarize students with the process of designing a cup car. These four tutorials will introduce students to many of the fundamentals of robotics, the software used to control the locomotion and sensors on an autonomous line following vehicle, and provide example code which help simplify the process of creating a competitive entry in the Freescale Cup. Here is an outline of the Basic Microcontroller Programming Tutorial: Read the microcontroller article Choose a microcontroller Set up the development environment Set up the microcontroller evaluation board Program A LED move to the next tutorial…
記事全体を表示
The line scan camera module consists of a CMOS linear sensor array of 128 pixels and an adjustable lens. This camera has a 1x128 resolution. Line Scan Camera Board Details Schematics, BOM, and datasheets: Line Scan Camera featuring TAOS 1401 Mounting Options You will likely want to mount the camera on a mast or boom above the car to ensure the greatest field of view. Determining the angle of orientation about the pivot at the top of the boom will change the “look ahead” distance of the camera and enable more efficient steering algorithms DIY Camera Mounts Solution Overview One method of implementation is to take the entire readout of the camera and store it in the memory. Then a line detection algorithm can be used to locate the position of the black line. Due to varying lighting conditions, some level of pixel thresholding may be necessary as the intensity differences across the data may not always produce a clear indication of the line location. A good approach is to use an algorithm that looks for changes in the magnitude of voltage from one portion of the array to another, since the camera’s AO magnitude is directly related to the brightness the pixel array senses. If the microcontroller finds a significant decrease in magnitude followed by large increase in magnitude this would give us a good indication of the location of the line. For this a derivative function can be utilized. Once we have successfully determined the position of the black line, immediately adjust the wheels to adjust the direction of the car so that the black line will remain in the center of the camera’s view. Sample camera output (for illustrative purposes only) The camera outputs an analog signal from 0 to 5V depending on the grey-scale value of the image. to simplify our sample we will assume that we have set limits for the line and have transformed the data to digital bits using a threshold value. 0’s are high intensity (non-line locations), 1’s are low intensity (black or line locations) 10000000000000000000000000000000001111101000000000000000000010000000000000000 Since the camera provides a 128x1 bit picture, and the camera will be pointing down at the track which is a fixed width. A control algorithm should be developed to line up the 1’s in the center of the 128 bits. The center of the field of view will be require calibration and testing, but it is assumed that the camera will remain in a fixed location pointing down the center of the forward looking axis of rotation. Signals For normal operation of the camera, the following signals must be produced and processed: CK (clock) - latches SI and clocks pixels out (low to high) continuous signal SI (serial input to sensor) begins a scan / exposure discrete pulses, pulse must go low before rising edge of next clock pulse AO (analog output) - Analog pixel input from the sensor (0-Vdd) or or tri-stated The CK and SI signals are simple ON/OFF signals which can be produce using a GPIO Pin, setting the pin high and low corresponding to the desired exposure time of the camera. The only other requirement is to read the Analog Output of the camera which requires the initialization of the Analog Module and setting it to the proper pinout. Acutal camera output image: Yellow = SI, Green = Camera Signal, Purple = clock More camera waveforms and information (Power Point) available here This link shows a video of the camera connected to the oscilloscope http://www.youtube.com/watch?v=YOAd3ERnXiQ To obtain this signal, connect channel 1, 2 and 3 of an oscilloscope to the SI pulse (Trigger off this signal), CLK, and AO signals. Timing The timing for creation and read of the signals is crucial and is detailed in the diagram below. This information can also be found in the Line Scan Datasheet. Analog Read: The Analog Output (AO) signal from the camera needs to be processed and read by the microcontroller's Analog to Digital Converter (ADC). This ADC device converts a continuous signal into a discrete number which is proportional to the signal voltage. An 8 bit ADC has 256 discrete levels (2^8). If a analog signal between 0 and 5 volts is sampled, a digital discrete number of 0 would correspond to zero volts, and a digital discrete number of 255 would correspond to 5 volts. A number such as 145w would correspond to about 2.8 volts. The maximum signal sample rate is limited by the microcontroller. Proper configuration of the ADC peripheral and the multiplexer of the chip will configure a pin to read in an analog signal when calling the function. More details on analog to digital converters can be found on the wikipedia site here. Read/Write In write mode, the GPIO pin can be set, cleared, or toggled via software initiated register settings. Microcontroller Reference Manual: Analog to Digital Converter You will find high level information about GPIO usage in several different areas of a reference manual. See the reference-manual article for more general information. Relevant Chapters: (see GPIO chapters for clock and SI Creation) Introduction: System Modules: System Integration Modules (SIM) - provides system control and chip configuration registers Chip Configuration: Signal Multiplexing: Port control and interrupts Focusing the camera: Once the sensor is perfectly working the next step is to find the best position of the lens that will generate the clearest images. The best way to do it is using an oscilloscope: Connect the SI and AO signals to the oscilloscope Set the SI pulse so that it can be clearly seen and then trig the AO signal with the SI signal using the trig function Fix the camera looking at a sheet of paper with a black line in the center The image of the black line will appear on the oscilloscope screen Screw the camera until you find the position where the line seems the clearest Camera Circuit   5 wires must be connected ground power SI CLK AO Camera Limitations   According to the datasheet:   " The sensor consists of 128 photodiodes arranged in a linear array. Light energy impinging on a photodiode generates photocurrent, which is integrated by the active integration circuitry associated with that pixel. During the intergration period, a sampling capacitor connects to the output of the integrator through an analog swith. The amount of charge accumulated at each pixel is directly proportional to the light intensity and the integration time." Integration Time: T T = (1/fmax)*(n-18)pixels + 20us, where n is the number of pixels Minimum integration time: 33.75us Maximum integration time: capacitors will saturate if exceeding 100ms frequency range 5 Khz - 8 Mhz (8 Mhz is fmax in equation above) The integration time is the following: It occurs between the 19th CLK cycle and the next SI pulse. The CLK frequency itself has little to do with the integration time. One each rising edge, the clock outputs one of the previously sampled intensity values. This means that integration time should be set by varying the time between SI pulses, not changing the clock frequency. Make the CLK frequency high, and have as much time as needed between the two SI pulses to obtain the desired intensity value. Pro Tips: #1 - Avoid Light Noise Light can be transmitted through the pcb on the back of the camera. This unwanted extra light shining on the CMOS linear sensor can induce significant errors into your signals received. A shroud or housing for the camera unit can easily eliminate this problem. One of the easiest solutions is to place a piece of electrical tape across the back of the camera in the highlighted area indicated in the picture below. #2 - Know your Settings When testing the car on the track or transporting it, it is not uncommon for the focus on the camera to loosen or change. Therefore it is recommended that after adjusting your camera focus for maximum performance you make mark (ex. metallic sharpie) between the lens and its body so you can realign the camera lens to it's proper position easily if it does shift. #3 - Know your Zone When hooking up the linescan camera, regardless of position or focus there is a drop off at each end of the image data. This is easily viewed with an oscilloscope. This effect is undesirable, particularly when you are finding your line position utilizing a derivative approach. These fallouts cause erroneous derivative values, and hence a poor line position solution. Two solutions we found useful were: (1) Ignoring the first 10-15 pixels and last 10-15 pixels of the image data array, and then determining the line position; (2) Often when making decisions in the code as to where the line was at it was found useful to use a threshold value for the difference in the derivative position, and secondly a binary threshold on the camera data. Note that the falloff depends on camera focus, position, etc. Therefore, these threshold values and pixels in which to ignore are relative to a specific instance. The problem however is common to the camera. #4 - Buffer Data Since the camera can read the line very quickly while the servo can only update every 20ms, there are multiple camera reads before the servo can update, if you are reading the camera fast and then overriding without saving them in some form then those camera reads are being wasted and are better off not having occurred. What can help is to create some sort of filter by bringing new values into an array with previous values and preforming some sort of averaging. The following code will take the new line position value and place it in a 1xA array where A is defined by CAMERA_AVG. NO AVERAGING IS OCCURRING HERE all that is happening is the camera values are being saved in a simple array, what is done with them is up to you. The way this works is that it shifts the entire array so the oldest data point is discarded in order to make room for the new line position at the other end of the array. It will only adds the new value if there is one available if not it copies the previous first position value to the new first position value. CAMERA_AVG => an integer value for how long the averaging length will occur gfpLineAverage => global floating point array of camera center line values fpLinePos => returned from read camera this is the center line position ReadCamera() => is the read camera function call returns a floating point value of fpLinePos // this will shift the values up and throw away the oldest value // then add a new reading for (i=CAMERA_AVG;i>0;i—) { gfpLineAverage[i]=gfpLineAverage[i-1]; } // if no line was detected the previous camera value will be passed on if (fpLinePos=ReadCamera()) { gfpLineAverage[0]= fpLinePos; } For example an array of of center line position values ranging from 0-127 could look like. Initial values [51 50 52 54 58 55] New position of 45 read [45 51 50 52 54 58] New position of 44 read [44 45 51 50 52 58] No value read [44 44 45 51 50 52] No value read [44 44 44 45 51 50] New position of 50 read [50 44 44 44 45 51] Program Exercise Specifics of how to configure the K40 ADC, to create the delay code is covered in the K40: Line Scan Camera Tutorial. Additional Training Resources Freescale Motor Control Tutorial Freescale Lecture 1: Introduction and Motor Basics Freescale Lecture 2: Pulse Width Modulaiton Freescale Lecture 3: Control Design Freesacle Lecture 4: Speed and Position Freescale Lecture 5: MPC5607B Overview Additional Resources Freescale app note on interfacing with a linescan camera Freescale app note on interfacing with an RCA camera
記事全体を表示
Have you even wondered where to get started when you wish to get support for your project? Here is a short presentation giving you the links to Project Sponsorship, Freescale Social Networks and other useful resources.
記事全体を表示
There are three types of memory in a typical Micrcontroller  FLASH - where your programs are stored RAM - for manipulating variables during runtime EEPROM - stores long term information
記事全体を表示
1. Overview 2. Hardware 3. Set up the Hardware: Line Scan Camera/Microcontroller Hardware Setup 4. Build the Code 5. Download/Debug/Run 6.Example Code Functions ImageCapture(); ReadADCChannel() Initialize the ADC Header File Definitions Initialize the GPIO Other Tutorials: This tutorial covers the details of obtaining data from the line scan camera on the Kinetis K40 using the TWR-K40X256-KIT evaluation board. General details of the line scan camera not related to the Kinetis can be found in the general Line Scan Camera Theory article. This tutorial will help students familiarize themselves with how to interface the camera with the microcontroller, how to configure GPIO pins to create clock signals and also how to utilize the microcontroller's ADC to read the data from the camera. Outside of control algorithms, configuring the camera is one of the more complex tasks necessary to create a Freescale Cup Vehicle. 1.  Overview In this exercise students will access the line scan camera, create a clock signal and create the initialization pulse which tells the camera to begin the exposure period. This tutorial will not describe line recognition or line following algorithms - these concepts are beyond its scope. Students will: Create the code using Codewarrior Build a project Download the code to the board connect the microcontroller to the camera. Run the program view the camera data, clock and Si pulse on an oscilloscope view the data from the camera in the CodeWarrior Debugger for verification purposes   To successfully complete this exercise, the following software and hardware are required: The K40 Tower card, TWR-K40x256 CodeWarrior for Microcontrollers Freescale Line Scan Camera Motor Board Tower Prototyping board Soldering Iron Solder Tower Elevators USB Cord 2. Hardware   Read the Line Scan Camera Overview article for general information on the camera, ADC, and GPIO microcontroller configuration settings. 3. Set up the Hardware: Line Scan Camera/Microcontroller Hardware Setup It is crucial for an engineer to have the proper test equipment and tools for the job. In this case, without an oscilloscope, students will not be able to verify whether the proper signals are being sent to the camera. 4. Build the Code If there is more than one project in your project view, make sure the proper project is the focus. The most reliable way to do this is to right click the project and choose Build Project as shown below. You can also go to the Project menu and choose the same command. If errors are encountered, look in the Problems view and resolve them. For now ignore any warnings. 5. Download/Debug/Run Download the code to your board, once this process is complete resume the project so that the code runs. If you want more information on how to complete this step see the download debug run section of the Kinetis Blinking Led tutorial. 6.Example Code What will happen: the function ImageCapture() is called in main.c with a pointer to the first element in the array. This function completes the processes necessary to capture images using the camera. To become more familiar with Pointers and Arrays - navigate to the C Programming Tutorial. Knowledge of Pointers and Arrays is a pre-requisite for understanding the Camera Code. Functions The camera code utilizes the following function: within main.c ImageCapture(&Line.RawCameraData[0]); is called to initiate the step of capturing an image into the first position of the array. ImageCapture(); from Camerainterface.c This function captures the images by creating the SI Pulse, and clock signals, capturing the data into an Array using the ADC features of the K40. It calls the function ReadADCChannel() at the proper time which then inputs data from the camera AO line. void ImageCapture(int * ImageData){//this is a pointer to a single character in memory   unsigned char i;   TAOS_SI_HIGH;   TAOS_EXPOSURE_DELAY;   TAOS_CLK_HIGH;   TAOS_EXPOSURE_DELAY;   TAOS_SI_LOW;   TAOS_EXPOSURE_DELAY;   ImageData[0] = (int)ReadADCChannel(19);// inputs data from camera (first pixel)   TAOS_CLK_LOW;   for(i=1;i<128;i++)   {   TAOS_EXPOSURE_DELAY;   TAOS_EXPOSURE_DELAY;   TAOS_CLK_HIGH;   TAOS_EXPOSURE_DELAY;   TAOS_EXPOSURE_DELAY;   ImageData[i] = (int)ReadADCChannel(19); // inputs data from camera (one pixel each time through loop)   TAOS_CLK_LOW;   }   TAOS_EXPOSURE_DELAY;   TAOS_EXPOSURE_DELAY;   TAOS_CLK_HIGH;   TAOS_EXPOSURE_DELAY;   TAOS_EXPOSURE_DELAY;   TAOS_CLK_LOW;  } ReadADCChannel() from readADC.c this function does the analog to digital conversion and returns a value between 0 and 255. It takes the proper ADC channel, in this case 19. Channel 19 corresponds to analog input pin ADC1_DM0 (see page 117 in the K40 Sub-Family Reference Manual). unsigned char ReadADCChannel(unsigned char Channel)   {   ADC1_SC1A = Channel;   while((ADC1_SC1A & ADC_SC1_COCO_MASK) == 0)   {   }   return ADC1_RA;    } Initialize the ADC Before utilizing the ADC it must be calibrated and initialized. The details for how to do this can be found in Chapter 19 Using Peripheral Delay Block (PDB) to Schedule Analog to Digital Converter (ADC) Conversions of the Kinetis Peripheral Module Quick Reference manual. The PDB portions of the code have been removed for the Cup Car Demo Code. Header File Definitions from k40_TOWER_BOARD_SUPPORT.h The following code enables the GPIO on the two pins: #define TAOS_CLK_LOC (1<<28) #define TAOS_SI_LOC (1<<18) Initialize the GPIO From K40_TOWER_BOARD_SUPPORT.c The InitK40GPIO Function sets up the ports for use: Relevant code SIM_SCGC5 = SIM_SCGC5_PORTA_MASK | SIM_SCGC5_PORTB_MASK | SIM_SCGC5_PORTC_MASK | SIM_SCGC5_PORTD_MASK | SIM_SCGC5_PORTE_MASK; //CLK and SI signal PORTC_PCR18 = PORT_PCR_MUX(1) | PORT_PCR_DSE_MASK; PORTE_PCR28 = PORT_PCR_MUX(1) | PORT_PCR_DSE_MASK; //Make Sure the GPIO is setup to be an output GPIOC_PDDR |= LED_E1_LOC | LED_E2_LOC | LED_E3_LOC | TAOS_SI_LOC; GPIOE_PDDR |= TAOS_CLK_LOC; GPIOB_PDDR |= LED_E4_LOC; Other Tutorials: K40:Blinking LED Tutorial K40:Drive DC Motor Tutorial K40:Turning a Servo Tutorial   
記事全体を表示
25 student teams from 21 universities coming from 11 countries will meet on 29-30 April for the Freescale Cup EMEA Challenge. Check out the event information at https://www.facebook.com/events/1425416907713292/
記事全体を表示
Overview The FRDM-TFC is a convenient "shield" that can drive up to two DC motors (5A per channel), two servos and I/O for the Freescale cup line scan camera and Hall effect sensors.  This board mates with the KL25Z Freedom board for primary usage with a Freescale Cup car. Features: 2 channel Motor Driver ICs (MC33887APVW) 2 channel servo Outputs Dual Linescan Camera interfaces Two inputs for speed sensors Two potentiometers for user functions Two push buttons for user functions 4 Position DIP Switch for user function 4 LEDs (green) for battery indicator or user functions Design Files Rev A is attached to this document. Rev B is attached to this document Code Examples Codewarrior "Bare Metal" Example Code: All Codewarrior based code examples for the FRDM-TFC are hosted on in a Subversion repository on Google Code: frdm-tfc -   Example code for the FRDM-TFC Shield - Google Project Hosting You can check out the code with your favorite SVN client.   Static releases are available in the attachments section of this page.  The current release is "R1.0" mbed.org Example Code: https://mbed.org/components/Freescale-Cup-with-FRDM-KL25Z/ Videos FRDM TFC EXAMPLE CODE GETTING STARTED FRDM-TFC_DEMO 0 and 1 FRDM-TFC_DEMO 2 and 3
記事全体を表示
Este es un teclado que tiene como propósito ayudar a las personas con problemas motrices, específicamente en las manos. Existen programas de diseño como photoshop o autocad en los cuales se puede ahorrar tiempo usando los macros con el teclado en lugar de usar el mouse para todo. KES tiene el propósito de ayudar a hacer más rápido el uso de estos programas y también ayudar a las personas con problemas motrices ya que con solo pulsar un botón será lo mismo que utilizar una combinación de los mismos. KES tiene la misión de agilizar el uso de macros en programas que conviene, aparte de el apoyo ofrecido a las personas con dificultades motrices. Enlace al video KES - YouTube
記事全体を表示
Getting Started with the NXP CUP These pages help you with the question of how to achieve the goal of creating an autonomous vehicle that quickly navigates around a track (timed race) and solves precision tasks (Figure 8, Speed limit zone, Obstacle avoidance) What is a Microcontroller? For information on what a microcontroller is head to the microcontrollers article. Getting Started - Learn to Program a microcontroller First off, you are going to need to know C programming. For a crash-course head to c-programming-for-embedded-systems. The classic first application to learn how to program a microcontroller is to get through the process of Blinking an LED. This wiki contains a tutorial for each of the Cup microprocessors which simplifies the process of setting up the evaluation board, installing the Integrated Development Environment, and programming the board with a simple set of software which blinks a LED. The Blink a LED tutorial is the first of 4 tutorials designed to familiarize students with the process of designing a cup car. These four tutorials will introduce students to many of the fundamentals of robotics, the software used to control the locomotion and sensors on an autonomous line following vehicle, and provide example code which help simplify the process of creating a competitive entry in the NXP CUP. Here is an outline of the Basic Microcontroller Programming Tutorial: Read the microcontroller article Choose a microcontroller Set up the development environment Set up the microcontroller evaluation board Program A LED move to the next tutorial… Course Material from the NXP CUP professors and supporters: Thanks to our professors and NXP CUP supporters we created an exclusive starter kit. It includes lecture material, information on the car, useful tips on the board etc. Download the file below and dive into a huge support portfolio! ARC Ingenierie Files - The Champions Board! ARC Ingenierie has been very generous in providing us with their PCB layout and Gerber files to produce your own NXP CUP board. They also provided sample code and drivers plus instructions (in French) to get you started. How cool is that?! Many thanks to ARC, this is much appreciated! Download the files below. If you want to build your own board, please contact us. When do so please keep in mind to give credit to ARC university. All boards should have "HE-ARC Ingenierie" inscription.   Further support links: Information on Line Scan Camera Use The Book of Eli - Microcontrollers, robotics and warp drives Microcontrollers MCU 101 - C Programming for Embedded Systems NXP CUP Shield for the FRDM KL25Z
記事全体を表示
Photos Videos
記事全体を表示
A tomada inteligente segue a filosofia proposta pelo protocolo internacional de medição e verificação (PIMVP) que diz “não gerenciamos aquilo que não medimos”. Porém, nem sempre temos um equipamento acessível ou recurso adequado para isso. A proposta da tomada é fornecer aos usuários um sistema de medição e controle sem a necessidade de grandes investimentos. O adaptador de tomada inteligente possui um circuito de medição de corrente elétrica e um circuito para medição da tensão elétrica presente na tomada. Estas informações são, inicialmente, armazenadas em na memória interna da tomada. Um aplicativo desenvolvido para dispositivos Android se comunica com a tomada, através da rede wireless da residência. Link do dropbox para acessar arquivos: Dropbox - Tomada Inteligente
記事全体を表示
Added by Gil Ernesto Rieke Aguirre on July 25, 2012 Universidad de Guadalajara test setup of Freescale Cup car. 
記事全体を表示