ユニバーシティ・プログラムのナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

University Programs Knowledge Base

ディスカッション

ソート順:
1. Overview   This module demonstrates how to implement a steering control system using Pulse Width Modulation (PWM) on NXP S32K3 microcontrollers. The application reads an analog input from a potentiometer (simulating a steering wheel) and converts it into a servo motor position. As the input changes, the servo motor reacts in real time, mimicking how steering systems work in modern vehicles. This example is based on Application Code Hub demonstrations for: PWM-Based Steering Control for FRDM-A-S32K344 PWM-Based Steering Control for FRDM-A-S32K312 In this workshop, a POT Click simulates the steering wheel position. When the student rotates it, an analog voltage proportional to the angle is read by the MCU through the ADC, scaled in software, and converted into a PWM duty cycle. The PWM is generated by the Servo Click (configured by the MCU over I²C) and drives a Micro Servo motor SG 180°, whose angle tracks the potentiometer in real time. Beyond the technical implementation, the course serves as a foundation for the Eat-Sleep-Code-Repeat learning initiative, encouraging a hands-on approach where students continuously learn, develop, test, and improve automotive embedded applications using real hardware and practical examples.   2. Learning Scope   After completing this course, participants should be able to:   Understand a basic steering control system and the ideas behind EPS and steer-by-wire. Use the POT Click as a simulated steering-wheel input. Acquire analog values (0–3.3 V) using the ADC and understand analog-to-digital conversion. Perform signal scaling from the ADC range to a servo angle / PWM duty cycle. Generate PWM signals to drive a servo motor. Configure the Servo Click over I²C using the OE (Output Enable) pin. Recognize the actuation data flow: sensor input → MCU processing → PWM actuation. Import, build, flash, and debug an ACH project in S32 Design Studio 3.6.5. Understand why steering functions are relevant for functional safety. 3. System Architecture   The three elements capture exactly the basic idea of the system in the demo: Input: Potentiometer (POT Click simulates the steering-wheel position) Processing: S32K3 MCU (reads the ADC, scales the value, commands the actuator) Output: Servo motor controlled via PWM (Micro Servo SG 180°) This matches the classic flow of an embedded actuation system: sensor → processing → actuator. Functional Flow The system operates continuously as follows: The potentiometer generates an analog voltage based on its position The ADC converts this voltage into a digital value The application scales this value into a steering angle The system generates a PWM signal based on the angle The servo motor moves accordingly This loop runs continuously to ensure real-time control. Steering Monitoring Application Architecture Steering Monitoring Application Architecture 4. Key Concepts   4.1 ADC (Analog-to-Digital Converter) The POT Click outputs 0–3.3 V depending on the wiper position. The ADC samples this voltage at regular intervals and quantizes it into a digital code (a 12-bit ADC produces values between 0 and 4095). The further the potentiometer is turned, the higher (or lower) the digital sample. ADC acquisition is the foundation of automotive sensing — used for torque, throttle, battery voltage, and many others. 4.2 Signal Scaling — From ADC to Servo Angle The ADC range (for example 0–4095) and the servo range (0°–180°, expressed as a PWM duty cycle) are different. The application performs a linear mapping so that one end of the potentiometer corresponds to one steering extreme and the other end to the opposite. This is the same scaling used in real EPS systems, where a hardware reading is converted into a normalized control command. 4.3 PWM — Pulse-Width Modulation and Servo Control PWM switches a digital output on and off at a fixed frequency, varying the duty cycle (the fraction of time the signal is high). A hobby servo such as the SG 180° interprets this duty cycle as a position command. In this demo, the PWM is not generated by the MCU itself but by the Servo Click's dedicated PWM controller, which the MCU configures over I²C — a typical embedded pattern that offloads time-critical signal generation and keeps the CPU free for application logic. 4.4 I²C — Configuring the Servo Click I²C — Inter-Integrated Circuit is a two-wire serial bus made of SDA (data) and SCL (clock). The S32K3 uses LPI2C1 on PTC6 (SDA) and PTC7 (SCL) to configure the Servo Click — PWM frequency, channel, and duty cycle. The OE — Output Enable pin on PTB17 is an additional control line that enables or disables the PWM outputs without reconfiguring the chip, which is also useful for a quick "safe stop" behavior. 4.5 POT Click as Steering Wheel The POT Click is a simplified, safe stand-in for a real steering sensor. The student rotates it by hand, the voltage changes, the MCU reads it through the ADC, scales it, and the servo reacts. 4.6 Data Flow at a Glance Physical rotation → analog voltage → ADC sample → scaled command (angle / duty cycle) → I²C configuration of the Servo Click → PWM signal → servo angle. This direct chain from the student's hand to the servo shaft is the main educational value of the demo. 5. Hardware and Software Setup   Required Hardware Component Image Purpose FRDM-A-S32K312 Alternative MCU platform used to run the steering application and process steering inputs. FRDM-A-S32K344 Alternative MCU platform used to run the steering application and control connected peripherals. FRDM-K64 Click Shield mikroBUS expansion board used to connect Click modules to the FRDM platform. Servo Click PWM driver board used to control the servo motor position. POT Click   Potentiometer module used to simulate steering wheel input. Micro Servo SG 180°                     Actuator used to convert control signals into steering movement. USB-C / 12 V supply — Provides power and enables programming and debugging of the system.   The example applications demonstrate how these peripherals are connected to the MCU pins and used to simulate steering wheel input and actuator control.   Steering Control Monitoring on FRDM-A-S32K312 Steering Control Monitoring on FRDM-A-S32K344       Software Environment S32 Design Studio IDE S32K3 Automotive Software Package Application Code Hub project import PWM-Based Steering Control for FRDM-A-S32K344 PWM-Based Steering Control for FRDM-A-S32K312 6. Implementation Guide   Step Action Sub-steps Expected Result 1 Import the Project Open S32 Design Studio Select “Import project from Application Code Hub” Search for the steering demo Use the GitHub link for automatic configuration Select main branch Import project Project successfully appears in workspace 2 Build the Application Right-click project Select “Update Code and Build Project” Confirm SDK component management Build completes with no errors and generates .elf file 3 Connect Hardware Connect USB cable (and 12V supply for S32K312) Attach click boards Verify wiring Board is powered and detected by IDE 4 Flash and Run Open Debug Configurations Select “debug_flash_pemicro” Start debugging Application runs continuously 5 Functional Validation Rotate the potentiometer Observe servo movement Servo follows potentiometer position in real time   7. Signal Behavior and Control Logic     Figure: Steering control signal mapping. The 12-bit ADC value (0–4095) is linearly mapped to a servo angle (0°–180°) and a matching PWM duty cycle (1.0–2.0 ms), with reference points at Left, Center and Right. At startup the servo moves to the neutral position; during operation, any input change produces an immediate, proportional reaction — implementing a basic steer-by-wire behavior.   8. Troubleshooting   Issue Possible Actions Board Not Detected Check USB cable and drivers Verify debugger connection Restart IDE No Servo Movement Verify PWM configuration Check servo wiring Ensure correct power supply Incorrect Behavior Check ADC configuration Validate scaling function Ensure PWM duty cycle mapping is correct Unstable Movement Add signal filtering Check power stability   9. Extending the Application   The basic implementation can be extended in several ways: Steering Range Control Restrict or extend the actuator's range of motion Define software-based limits to protect the mechanics Input Direction Inversion Reverse how the actuator responds to the input Useful for left-hand vs. right-hand drive calibration Noise Filtering Apply software filtering to stabilize readings Avoid jitter near the center position Scaling Logic Exploration Identify and analyze how the input is mapped to the output Connect software math with hardware behavior Fault-Handling Behavior Add a mechanism that reacts to a detected fault Transition the system into a safer state State Machine Implementation A more advanced approach is to implement a state machine: Idle Active Fault 10. Safety Context   This example reflects key automotive principles: Continuous monitoring of driver input Immediate response to control signals Reliable actuator control In real systems: Redundancy is required Fault detection mechanisms are implemented Systems must comply with ISO 26262 (functional safety standard) Steer-by-wire systems require high reliability since there is no direct mechanical link. 11. Conclusion   This module demonstrates how a simple embedded system can implement steering control using ADC input and PWM output. It shows how: Analog input is acquired Data is processed in real time Actuators are controlled using PWM   Result on FRDM-A-S32K312 Result on FRDM-A-S32K344 Steering demo result on FRDM-A-S32K312 Steering demo result on FRDM-A-S32K344   The course provides a strong foundation for more advanced systems, including filtering, state machines, and safety-oriented designs.
記事全体を表示
The course serves as a foundation for the Eat-Sleep-Code-Repeat learning initiative, encouraging a hands-on approach where students continuously learn, develop, test, and improve automotive embedded applications using real hardware and practical examples.
記事全体を表示
The course serves as a foundation for the Eat-Sleep-Code-Repeat learning initiative, encouraging a hands-on approach where students continuously learn, develop, test, and improve automotive embedded applications using real hardware and practical examples.
記事全体を表示
The course serves as a foundation for the Eat-Sleep-Code-Repeat learning initiative, encouraging a hands-on approach where students continuously learn, develop, test, and improve automotive embedded applications using real hardware and practical examples.
記事全体を表示
1. Overview   This module demonstrates how to implement a vehicle lighting control system using analog input acquisition and FlexIO-based LED driving on NXP S32K3 microcontrollers. The application reads analog inputs from the Analog Key Click module (six push-buttons, each generating a distinct voltage level) and converts them into commands that drive a 4x4 RGB LED matrix. Each button press activates a specific lighting function — low beam, high beam, turn signals, brake lights, or hazard lights — while safety interlocks and blinking patterns run continuously in the background, mimicking how a real automotive Body Control Module (BCM) manages vehicle lighting. This example is based on Application Code Hub demonstrations for: Vehicle Lighting Control for Daylight and Hazard Signals on FRDM-A-S32K344 Vehicle Lighting Control for Daylight and Hazard Signals on FRDM-A-S32K312 In this workshop, the Analog Key Click simulates six vehicle lighting controls. When the student presses a button, an analog voltage proportional to the pressed key is read by the MCU through the ADC (with software debouncing), decoded into a specific lighting command, and translated into an RGB pattern generated by the FlexIO peripheral. The 4x4 RGB Click then displays the corresponding automotive lighting behavior in real time — warm white for low beams, cool white for high beams, blinking amber for turn signals and hazards, and red for brake lights. Beyond the technical implementation, the course serves as a foundation for the Eat-Sleep-Code-Repeat learning initiative, encouraging a hands-on approach where students continuously learn, develop, test, and improve automotive embedded applications using real hardware and practical examples.   2. Learning Scope   After completing this course, participants should be able to:   Understand a basic vehicle lighting control system and the ideas behind an automotive Body Control Module (BCM). Use the Analog Key Click as a simulated multi-button user interface (six inputs on a single analog line). Acquire analog values (0–3.3 V) using the ADC and understand how multiple buttons share one channel through voltage division. Perform software debouncing and decode which button was pressed based on ADC value ranges. Drive an RGB LED matrix using the FlexIO peripheral, generating precise timing for WS2812-style LEDs. Implement safety interlocks between lighting functions (e.g., high beam requires low beam ON). Implement continuous background patterns such as blinking turn signals and synchronized hazards. Recognize the actuation data flow: analog input → ADC → command decoding → FlexIO LED output. Import, build, flash, and debug an ACH project in S32 Design Studio 3.6.5. Understand why lighting functions are relevant for automotive safety and driver visibility. 3. System Architecture   The three elements capture exactly the basic idea of the system in the demo: Input: Analog Key Click (six buttons T1–T6, each generating a distinct analog voltage level) Processing: S32K3 MCU (reads the ADC, decodes the button, applies BCM logic, updates the LED state) Output: 4x4 RGB Click (16-LED matrix driven by FlexIO to display lighting patterns) This matches the classic flow of an embedded body-control system: sensor → processing → actuator. Functional Flow The system operates continuously as follows: The user presses a button on the Analog Key Click (T1–T6) Each button generates a distinct analog voltage on the shared output line The ADC samples the voltage and converts it into a digital value The application decodes which button was pressed (with debouncing) The BCM logic applies interlocks and dependencies (e.g., high beam requires low beam) The FlexIO peripheral drives the RGB Click LEDs with the corresponding color pattern This loop runs continuously to ensure real-time lighting control, with blinking patterns and safety interlocks maintained in the background. Vehicle Lighting Control Application Architecture    4. Key Concepts   4.1 ADC (Analog-to-Digital Converter) The Analog Key Click outputs 0–3.3 V on a single analog line, with each button generating a specific voltage step. The ADC samples this voltage on ADC0_P0 (pin PTD1) at regular intervals and quantizes it into a digital code (a 12-bit ADC produces values between 0 and 4095). Each button corresponds to a specific value range, allowing six digital inputs to be read through a single ADC channel. ADC acquisition is the foundation of automotive sensing — used for switches, buttons, sensors, and many others. 4.2 Analog Multi-Button Decoding Instead of using six separate GPIO pins, the Analog Key Click uses a resistor ladder that produces a different voltage for each button press. The application performs software debouncing (multiple ADC samples must agree before a press is confirmed) and then compares the ADC value against predefined thresholds to identify which button (T1–T6) was pressed. This technique is common in automotive steering-wheel controls, where many buttons share a single analog line to save wiring and pins. 4.3 FlexIO — Driving the RGB Click LEDs FlexIO is a highly flexible peripheral on S32K3 that can emulate serial protocols like WS2812/NeoPixel. The RGB Click uses individually addressable LEDs that require precise timing (~800 kHz with strict pulse widths). FlexIO on PTA13 (FlexIO_D8) generates this waveform in hardware, without loading the CPU. Each of the 16 LEDs receives its color data through a serial stream, allowing independent control of color and brightness per LED. 4.4 RGB LED Mapping and Lighting Zones The 16 LEDs of the RGB Click are logically grouped into automotive lighting zones: LEDs 13, 14 → Low Beam Headlights (warm white) LEDs 8, 9, 10, 11 → High Beam Headlights (cool white) LEDs 0, 12 → Left Turn Signal (blinking amber) LEDs 3, 15 → Right Turn Signal (blinking amber) LEDs 1, 2, 5, 6 → Brake Lights (red) LEDs 0, 3, 12, 15 → Hazard Lights (synchronized blinking amber) 4.5 BCM Safety Interlocks and State Dependencies The application implements safety logic typical of a real Body Control Module: high beam can only be activated when low beam is already ON; turning OFF the low beam automatically disables the high beam; hazard lights synchronize left and right turn signals simultaneously; high beam state is preserved during hazard blinking and restored between cycles. These interlocks illustrate how real automotive lighting logic prevents unsafe combinations and preserves driver intent. 4.6 Data Flow at a Glance Button press → analog voltage on shared line → ADC sample → software debouncing → button decoding → BCM logic (interlocks + dependencies) → FlexIO WS2812 output stream → RGB LED color update. This direct chain from the student's finger to the LEDs is the main educational value of the demo. 5. Hardware and Software Setup   Required Hardware Component Image Purpose FRDM-A-S32K312 Alternative MCU platform used to run the lighting application and process user inputs. FRDM-A-S32K344 Alternative MCU platform used to run the lighting application and control connected peripherals. FRDM-K64 Click Shield mikroBUS expansion board used to connect Click modules to the FRDM platform. Analog Key Click Six-button analog module used to simulate the vehicle lighting controls (headlights, indicators, brakes, hazards). 4x4 RGB Click 16-LED RGB matrix used to display the automotive lighting patterns in real time. USB-C / 12 V supply — Provides power and enables programming and debugging of the system through a single USB-C connection.   The example applications demonstrate how these peripherals are connected to the MCU pins and used to simulate a complete vehicle lighting control system.   Vehicle Lighting Control on FRDM-A-S32K312 Vehicle Lighting Control on FRDM-A-S32K344   Software Environment S32 Design Studio IDE S32K3 Automotive Software Package Application Code Hub project import Vehicle Lighting Control for Daylight and Hazard Signals on FRDM-A-S32K344 Vehicle Lighting Control for Daylight and Hazard Signals on FRDM-A-S32K312 6. Implementation Guide   Step Action Sub-steps Expected Result 1 Import the Project Open S32 Design Studio 3.6.5 Select “Import project from Application Code Hub” Search for “Lighting” Select the desired project for your FRDM board Use the GitHub link for automatic configuration Select main branch Import project Project successfully appears in workspace 2 Build the Application Right-click project Select “Update Code and Build Project” Confirm SDK component management Build completes with no errors and generates .elf file 3 Connect Hardware Connect USB-C cable (and 12 V supply for FRDM-A-S32K312) Attach FRDM-K64 Click Shield, Analog Key Click and 4x4 RGB Click Verify wiring on PTA13 (FlexIO) and PTD1 (ADC) Board is powered and detected by IDE 4 Flash and Run Open Debug Configurations Select “debug_flash_pemicro” Start debugging Application runs continuously; LEDs perform startup test sequence 5 Functional Validation Press buttons T1–T6 on the Analog Key Click Observe corresponding LED patterns on the RGB Click Verify safety interlocks (high beam requires low beam) Verify continuous blinking on turn signals and hazards RGB LEDs display the correct automotive lighting patterns for each button   7. Signal Behavior and Control Logic   The following diagram illustrates how each user input on the Analog Key Click is mapped to a specific lighting function and to the individual LEDs of the 4×4 RGB Click matrix. Each button (T1–T6) triggers a unique combination of LEDs, colors, and patterns, reproducing the behavior of a simplified automotive lighting system.    The MCU continuously monitors the analog input from the Analog Key Click and decodes which button is pressed. Based on the detected input, the application activates the corresponding lighting function by driving the assigned LEDs on the 4×4 RGB Click through the FlexIO serial interface. Steady functions (Low Beam, High Beam, Brake) keep the associated LEDs constantly ON, while directional functions (Left Turn, Right Turn, Hazard) toggle the LEDs at approximately 1 Hz to reproduce the blinking behavior of real vehicle indicators. Additional control rules — such as High Beam requiring Low Beam to be active, or Hazard Lights preserving and restoring the High Beam state — reflect the interdependencies found in a real automotive body control module.   8. Troubleshooting   Issue Possible Actions Board Not Detected Check USB-C cable and drivers Verify debugger connection Restart IDE No LEDs Lighting Up Verify FlexIO configuration on PTA13 Check 3.3 V and GND wiring on RGB Click Confirm data-line wiring to IN1 Buttons Not Detected Verify ADC0_P0 configuration on PTD1 Check 3.3 V and GND wiring on Analog Key Click Confirm software debouncing thresholds Wrong Button Triggered Recalibrate ADC value ranges for each button Verify power supply stability (3.3 V) Check for noise on the analog line Incorrect LED Colors or Timing Verify FlexIO clock configuration (WS2812 timing) Check LED index → color mapping in code Ensure RGB order (GRB vs. RGB) matches the LED type High Beam Not Activating Ensure low beam (T1) is ON first — BCM interlock Check application logic for beam dependencies   9. Extending the Application   The basic implementation can be extended in several ways: Additional Lighting Functions Add fog lights, parking lights, or daytime running lights (DRL) Simulate reverse lights that activate when a specific input is triggered Adaptive Front Lighting Integrate a steering angle input (e.g., POT Click) to swivel the headlights Simulate cornering lights that turn on when indicators are active Ambient Light Sensing Add a light sensor to automatically enable low beams at dusk Implement smooth dimming between day and night modes Brake Light Enhancements Add an emergency brake flashing pattern for hard braking Implement a third brake light (single LED, always ON with brakes) CAN Communication Enable communication with other vehicle ECUs (e.g., BCM master, doors) Receive lighting commands over the vehicle network State Machine Implementation A more advanced approach is to implement a formal state machine covering: Off DRL / Parking Low Beam High Beam Hazard / Fault 10. Safety Context   This example reflects key automotive principles: Continuous monitoring of driver input Immediate response to control signals Reliable actuator (LED) control with predictable timing Safety interlocks between lighting functions (high beam requires low beam) In real systems: Redundancy is required for safety-relevant functions (e.g., brake lights, hazards) Fault detection mechanisms are implemented (open lamp, short circuit, overcurrent) Systems must comply with ISO 26262 (functional safety standard) Vehicle lighting is one of the most safety-critical automotive functions because it directly affects driver visibility and vehicle conspicuity. Modern Body Control Modules implement extensive diagnostics, backup lighting strategies, and fail-safe defaults (e.g., hazard lights activated on power-loss recovery). 11. Conclusion   This module demonstrates how a simple embedded system can implement complete vehicle lighting control using ADC input and FlexIO output on the S32K3 platform. It shows how: Multiple digital inputs can share a single analog line through resistor-ladder decoding Analog data is acquired, debounced and processed in real time Complex automotive lighting patterns are controlled through FlexIO-driven WS2812 LEDs Safety interlocks and background blinking patterns are managed by BCM-style logic   Result on FRDM-A-S32K312 Result on FRDM-A-S32K344 FRDM-A-S32K312 FRDM-A-S32K344   The course provides a strong foundation for more advanced systems, including adaptive lighting, CAN networking, ambient sensing, and safety-oriented designs typical of automotive body-control modules.
記事全体を表示
Continue discussion on the line scan camera. A completely interrupt driven approach to the interface will be illustrated.
記事全体を表示
Harvard Extension School CSCI E-251, Fall 2012: Principles of Operating Systems Final Project Presentations Presentation by Ram Garlapati
記事全体を表示
Harvard Extension School CSCI E-251, Fall 2012: Principles of Operating Systems Final Project Presentations Presentation by Eric Pedersen
記事全体を表示
In this video we will look at the example code provided for the FRDM-TFC for use with the mbed development environment. Alternatively, you can see the same example code as it is used with CodeWarrior here:
記事全体を表示
Harvard Extension School CSCI E-251, Fall 2012: Principles of Operating Systems Final Project Presentations Presentation by Ethan Tavan
記事全体を表示
Review the design and operation of the Freescale linescan camera included with the TFC-KIT. A high level overview of the sensor IC interface will be shown to the audience. View Video Link : 1471 and Video Link : 1472
記事全体を表示
Harvard Extension School CSCI E-251, Fall 2012: Principles of Operating Systems Final Project Presentations Presentation by Timothy O'Keefe
記事全体を表示
Entrenamiento sobre ADC del Kinetis L Series. Encuentra el material completo en https://community.freescale.com/docs/DOC-95205
記事全体を表示
The Freescale Cup has been around the world for the last 9 years. Over 23,000 students work each year on intelligent cars to make then run around the track at fast speed. Find more information on the community. Select the region you are part on and engage in the next season of the challenge.
記事全体を表示
Entrenamiento acerca del MCG de la herramienta de desarrollo Freedom, para los microcontroladores Kinetis L series. Para acceder al material completo visita: https://community.freescale.com/docs/DOC-95205
記事全体を表示
In this two part series we take a deeper look at the inner workings of a microcontroller. This video will examine a "generic" microcontroller. Components that are common to most microcontrollers will be examine.   View Video Link : 1453
記事全体を表示
En este video puedes consultar paso a paso la descarga e instalación del CodeWarrior 10.4 para microcontroladores. Accede a la liga www.freescale.com/cwmcu10
記事全体を表示
Find the complete material at: https://community.freescale.com/docs/DOC-95205
記事全体を表示
Freescale Cup shield introduction for use with the FRDM-KL25Z or similar development board. Steps through the schematic of the FRDM-TFC shield and explain it's interfaces, logic, and use.
記事全体を表示
In this video, we will examine a commercial of the shelf (COTS) H-Bridge IC. Example code for the FRDM-TFC will also be examined.
記事全体を表示