USDPAA Support in YoctoProject

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USDPAA Support in YoctoProject

ソリューションへジャンプ
5,509件の閲覧回数
ramkrishnan
Contributor III

THe last SDK2.0 release for the T1024 processor was in March 2017. Will there be a new one with the later yoctoproject release for eg dunfell.

Related to this is a question regarding USDPAA support for the T1024. The dunfell project does not seem to have any support for USDPAA. Is this maintained by NXP to be released in an SDK ?

 

Thanks,

Ram Krishnan

 

ラベル(1)
0 件の賞賛
返信
1 解決策
5,500件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

This release https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk/tree/readme?h=dunfell is the latest Yocto SDK release for T1024RDB form NXP, however there is no USDPAA support in this release.

If you want to use USDPAA, you have to use QorIQ Linux SDK 2.0 1703 release.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
5,501件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

This release https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk/tree/readme?h=dunfell is the latest Yocto SDK release for T1024RDB form NXP, however there is no USDPAA support in this release.

If you want to use USDPAA, you have to use QorIQ Linux SDK 2.0 1703 release.

0 件の賞賛
返信
5,284件の閲覧回数
ramkrishnan
Contributor III

Based on this topic. Will DPDK support T1024 ?  If not , what method can I use to do network packet processing on the T1024. USDPAA has been discontinued.

 

Ram

 

0 件の賞賛
返信
5,492件の閲覧回数
ramkrishnan
Contributor III

Thank you , is there any plan port over usdpaa to the newer branch.

 

Ram Krishnan

0 件の賞賛
返信