USDPAA Support in YoctoProject

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USDPAA Support in YoctoProject

Jump to solution
5,498 Views
ramkrishnan
Contributor III

THe last SDK2.0 release for the T1024 processor was in March 2017. Will there be a new one with the later yoctoproject release for eg dunfell.

Related to this is a question regarding USDPAA support for the T1024. The dunfell project does not seem to have any support for USDPAA. Is this maintained by NXP to be released in an SDK ?

 

Thanks,

Ram Krishnan

 

Labels (1)
0 Kudos
Reply
1 Solution
5,489 Views
yipingwang
NXP TechSupport
NXP TechSupport

This release https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk/tree/readme?h=dunfell is the latest Yocto SDK release for T1024RDB form NXP, however there is no USDPAA support in this release.

If you want to use USDPAA, you have to use QorIQ Linux SDK 2.0 1703 release.

View solution in original post

0 Kudos
Reply
3 Replies
5,490 Views
yipingwang
NXP TechSupport
NXP TechSupport

This release https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk/tree/readme?h=dunfell is the latest Yocto SDK release for T1024RDB form NXP, however there is no USDPAA support in this release.

If you want to use USDPAA, you have to use QorIQ Linux SDK 2.0 1703 release.

0 Kudos
Reply
5,273 Views
ramkrishnan
Contributor III

Based on this topic. Will DPDK support T1024 ?  If not , what method can I use to do network packet processing on the T1024. USDPAA has been discontinued.

 

Ram

 

0 Kudos
Reply
5,481 Views
ramkrishnan
Contributor III

Thank you , is there any plan port over usdpaa to the newer branch.

 

Ram Krishnan

0 Kudos
Reply