T4240 endpoint problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T4240 endpoint problem

Jump to solution
2,665 Views
emilviding
Contributor I

Hi,

I have a T4240 processor with PCIe1 configured as endpoint (HOST_AGT_PEX = 010).

The endpoint is connected to a PCIe switch. The Root Complex is a P1022.

I can't make any configuration accesses towards the T4240 EP, all I can see in my Lauterbach window is ????????. When I disable the controller in the DEVDISR register I read all ones.

Is there anything I need to do for the enpoint to answer configuration accesses? I have used P1022 and P4080 before and then you just have to turn the power on.

Regards,

Emil Viding

HW designer

Saab

Labels (1)
0 Kudos
Reply
1 Solution
2,451 Views
ufedor
NXP Employee
NXP Employee

> Is there anything I need to do for the endpoint to answer configuration accesses?

Please check that CONFIG[CFG_READY] is set.

View solution in original post

0 Kudos
Reply
2 Replies
2,452 Views
ufedor
NXP Employee
NXP Employee

> Is there anything I need to do for the endpoint to answer configuration accesses?

Please check that CONFIG[CFG_READY] is set.

0 Kudos
Reply
2,451 Views
emilviding
Contributor I

Well this is embarrassing... That solved it, thanks!

/Emil

0 Kudos
Reply