T4240 endpoint problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

T4240 endpoint problem

跳至解决方案
2,657 次查看
emilviding
Contributor I

Hi,

I have a T4240 processor with PCIe1 configured as endpoint (HOST_AGT_PEX = 010).

The endpoint is connected to a PCIe switch. The Root Complex is a P1022.

I can't make any configuration accesses towards the T4240 EP, all I can see in my Lauterbach window is ????????. When I disable the controller in the DEVDISR register I read all ones.

Is there anything I need to do for the enpoint to answer configuration accesses? I have used P1022 and P4080 before and then you just have to turn the power on.

Regards,

Emil Viding

HW designer

Saab

标签 (1)
0 项奖励
回复
1 解答
2,443 次查看
ufedor
NXP Employee
NXP Employee

> Is there anything I need to do for the endpoint to answer configuration accesses?

Please check that CONFIG[CFG_READY] is set.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,444 次查看
ufedor
NXP Employee
NXP Employee

> Is there anything I need to do for the endpoint to answer configuration accesses?

Please check that CONFIG[CFG_READY] is set.

0 项奖励
回复
2,443 次查看
emilviding
Contributor I

Well this is embarrassing... That solved it, thanks!

/Emil

0 项奖励
回复