T4240 endpoint problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T4240 endpoint problem

ソリューションへジャンプ
2,669件の閲覧回数
emilviding
Contributor I

Hi,

I have a T4240 processor with PCIe1 configured as endpoint (HOST_AGT_PEX = 010).

The endpoint is connected to a PCIe switch. The Root Complex is a P1022.

I can't make any configuration accesses towards the T4240 EP, all I can see in my Lauterbach window is ????????. When I disable the controller in the DEVDISR register I read all ones.

Is there anything I need to do for the enpoint to answer configuration accesses? I have used P1022 and P4080 before and then you just have to turn the power on.

Regards,

Emil Viding

HW designer

Saab

ラベル(1)
0 件の賞賛
返信
1 解決策
2,455件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Is there anything I need to do for the endpoint to answer configuration accesses?

Please check that CONFIG[CFG_READY] is set.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,456件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Is there anything I need to do for the endpoint to answer configuration accesses?

Please check that CONFIG[CFG_READY] is set.

0 件の賞賛
返信
2,455件の閲覧回数
emilviding
Contributor I

Well this is embarrassing... That solved it, thanks!

/Emil

0 件の賞賛
返信