T2080 KERNEL can not startup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080 KERNEL can not startup

ソリューションへジャンプ
2,732件の閲覧回数
tapyang
Contributor III

Hi, Dear Experts:

When I am developping my custom T2080 board, the U-BOOT has startup normally.

Then, I download the kernel uImage, FileSystem and dtb, However, It can not start up, and die at:

pastedImage_1.png

The attachment is the startup log!

Expect your reply and thank you very much!

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,493件の閲覧回数
tapyang
Contributor III

I have solved this question,thx!~

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,494件の閲覧回数
tapyang
Contributor III

I have solved this question,thx!~

0 件の賞賛
返信
2,493件の閲覧回数
sandratrujillog
Contributor III

I have the same question, How did you solved it?

Thanks!

0 件の賞賛
返信
2,493件の閲覧回数
tapyang
Contributor III

The startup config's fault! I excute the command " setenv bootargs ‘root=/dev/ram0 earlycon=uart8250,mmio,0x21c0500 console=ttyS0,115200’
"

Then, It is Okay!