T2080 KERNEL can not startup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

T2080 KERNEL can not startup

跳至解决方案
2,712 次查看
tapyang
Contributor III

Hi, Dear Experts:

When I am developping my custom T2080 board, the U-BOOT has startup normally.

Then, I download the kernel uImage, FileSystem and dtb, However, It can not start up, and die at:

pastedImage_1.png

The attachment is the startup log!

Expect your reply and thank you very much!

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,473 次查看
tapyang
Contributor III

I have solved this question,thx!~

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,474 次查看
tapyang
Contributor III

I have solved this question,thx!~

0 项奖励
回复
2,473 次查看
sandratrujillog
Contributor III

I have the same question, How did you solved it?

Thanks!

0 项奖励
回复
2,473 次查看
tapyang
Contributor III

The startup config's fault! I excute the command " setenv bootargs ‘root=/dev/ram0 earlycon=uart8250,mmio,0x21c0500 console=ttyS0,115200’
"

Then, It is Okay!