Multicore Application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multicore Application

1,641 Views
avinashneethi
Contributor I

Hi,


Any sample application code is available to teset T4241 Multiple core.


Regards,
Avinash N

0 Kudos
Reply
1 Reply

1,520 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Avinash N,

You could create a bareboard project for T4240 in CodeWarrior IDE following new project wizards, in the Configurations panel, please select SMP and select Core index for all cores. Then connect CodeWarrior to the target board to execute the sample program at all cores.

In addition, in Debug Target Settings panel, please select "Download SRAM" or "Connect SRAM" Launch configuration to avoid DDR controller configuration trouble.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply