T2080 Flash Timing Register

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080 Flash Timing Register

2,492件の閲覧回数
anshulkhare
Contributor III

Hi!

I am using T2080 board and interfacing NOR Flash to IFC.

i am confused in IFC Flash Timing Registers. I have read the reference manual but i can not decide that what values should i set in all timing registers and what is the value of ip clk and IFC module input clocks that is used in reference manual.

Thank you

Regards,

Anshul Khare

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,303件の閲覧回数
ufedor
NXP Employee
NXP Employee

> what values should i set in all timing registers

Please refer to the attached CodeWarrior initialization script for the T2080RDB - it contains IFC registers initialization.

> what is the value of ip clk and IFC module

For the IFC ip_clk (IFC module input clock) refer to the T2080 Reference manual, Figure 4-3. T2080 Logic Clock Subsystem Block Diagram - 1/2 Platform clk.

For the IFC clock (IFC_CLK) frequency refer to the T2080 Reference manual, 13.3.32 Clock Control register (IFC_CCR), CLKDIV

0 件の賞賛
返信

2,303件の閲覧回数
anshulkhare
Contributor III

Hello ufedor‌

Thanks for reply.

CodeWarrior initialization script for the T2080RDB is not attached in your reply.

please provide the same.

Regards,

Anshul Khare

0 件の賞賛
返信

2,303件の閲覧回数
ufedor
NXP Employee
NXP Employee

Definitely it is attached - please see the screenshot:

2018-10-09_135706.jpg

0 件の賞賛
返信

2,303件の閲覧回数
anshulkhare
Contributor III

yes got it.

Thanks :smileyhappy:

0 件の賞賛
返信