T2080 Flash Timing Register

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T2080 Flash Timing Register

2,490 次查看
anshulkhare
Contributor III

Hi!

I am using T2080 board and interfacing NOR Flash to IFC.

i am confused in IFC Flash Timing Registers. I have read the reference manual but i can not decide that what values should i set in all timing registers and what is the value of ip clk and IFC module input clocks that is used in reference manual.

Thank you

Regards,

Anshul Khare

标签 (1)
0 项奖励
回复
4 回复数

2,301 次查看
ufedor
NXP Employee
NXP Employee

> what values should i set in all timing registers

Please refer to the attached CodeWarrior initialization script for the T2080RDB - it contains IFC registers initialization.

> what is the value of ip clk and IFC module

For the IFC ip_clk (IFC module input clock) refer to the T2080 Reference manual, Figure 4-3. T2080 Logic Clock Subsystem Block Diagram - 1/2 Platform clk.

For the IFC clock (IFC_CLK) frequency refer to the T2080 Reference manual, 13.3.32 Clock Control register (IFC_CCR), CLKDIV

0 项奖励
回复

2,301 次查看
anshulkhare
Contributor III

Hello ufedor‌

Thanks for reply.

CodeWarrior initialization script for the T2080RDB is not attached in your reply.

please provide the same.

Regards,

Anshul Khare

0 项奖励
回复

2,301 次查看
ufedor
NXP Employee
NXP Employee

Definitely it is attached - please see the screenshot:

2018-10-09_135706.jpg

0 项奖励
回复

2,301 次查看
anshulkhare
Contributor III

yes got it.

Thanks :smileyhappy:

0 项奖励
回复