T2080 Flash Timing Register

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 Flash Timing Register

2,491 Views
anshulkhare
Contributor III

Hi!

I am using T2080 board and interfacing NOR Flash to IFC.

i am confused in IFC Flash Timing Registers. I have read the reference manual but i can not decide that what values should i set in all timing registers and what is the value of ip clk and IFC module input clocks that is used in reference manual.

Thank you

Regards,

Anshul Khare

Labels (1)
0 Kudos
Reply
4 Replies

2,302 Views
ufedor
NXP Employee
NXP Employee

> what values should i set in all timing registers

Please refer to the attached CodeWarrior initialization script for the T2080RDB - it contains IFC registers initialization.

> what is the value of ip clk and IFC module

For the IFC ip_clk (IFC module input clock) refer to the T2080 Reference manual, Figure 4-3. T2080 Logic Clock Subsystem Block Diagram - 1/2 Platform clk.

For the IFC clock (IFC_CLK) frequency refer to the T2080 Reference manual, 13.3.32 Clock Control register (IFC_CCR), CLKDIV

0 Kudos
Reply

2,302 Views
anshulkhare
Contributor III

Hello ufedor‌

Thanks for reply.

CodeWarrior initialization script for the T2080RDB is not attached in your reply.

please provide the same.

Regards,

Anshul Khare

0 Kudos
Reply

2,302 Views
ufedor
NXP Employee
NXP Employee

Definitely it is attached - please see the screenshot:

2018-10-09_135706.jpg

0 Kudos
Reply

2,302 Views
anshulkhare
Contributor III

yes got it.

Thanks :smileyhappy:

0 Kudos
Reply