T2080 Basic boot code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 Basic boot code

2,700 Views
Faizanbaig
Contributor IV

Hi,

We are trying to initialize stack, CPU , RAM on T2080ARDB but we are not finding basic baremetal boot code for initialization.

Could you please help us with any pointers or reference to look into?

 

Thanks,

Faizanbaig Inamdar

Labels (1)
Tags (2)
0 Kudos
Reply
3 Replies

2,694 Views
ufedor
NXP Employee
NXP Employee

There are no such separate software components from NXP.

Available complex reference is U-Boot source code from the Linux SDK.

The SDK v2.0 can be downloaded from:

http://www.nxp.com/products/software-and-tools/run-time-software/linux-sdk/linux-sdk-for-qoriq-proce...

0 Kudos
Reply

2,682 Views
Faizanbaig
Contributor IV

Thanks for the response.

I installed SDK on linux and my need is to get start.S file for T2080rdb e6500 core.

I migrated to below path after sdk installation:

/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b/tmp/work/t2080rdb_64b-fsl-linux/u-boot-qoriq/2016.09+fslgit-r0/git/arch/powerpc

I couldnt find the start.S for e6500 power pc core .

Could you please suggest something?

Thanks.

0 Kudos
Reply

2,678 Views
ufedor
NXP Employee
NXP Employee

The same "start.S" is used for all processors of the "mpc85xx" branch including T2080.

0 Kudos
Reply