T2080 Basic boot code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080 Basic boot code

2,680件の閲覧回数
Faizanbaig
Contributor IV

Hi,

We are trying to initialize stack, CPU , RAM on T2080ARDB but we are not finding basic baremetal boot code for initialization.

Could you please help us with any pointers or reference to look into?

 

Thanks,

Faizanbaig Inamdar

ラベル(1)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,674件の閲覧回数
ufedor
NXP Employee
NXP Employee

There are no such separate software components from NXP.

Available complex reference is U-Boot source code from the Linux SDK.

The SDK v2.0 can be downloaded from:

http://www.nxp.com/products/software-and-tools/run-time-software/linux-sdk/linux-sdk-for-qoriq-proce...

0 件の賞賛
返信

2,662件の閲覧回数
Faizanbaig
Contributor IV

Thanks for the response.

I installed SDK on linux and my need is to get start.S file for T2080rdb e6500 core.

I migrated to below path after sdk installation:

/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b/tmp/work/t2080rdb_64b-fsl-linux/u-boot-qoriq/2016.09+fslgit-r0/git/arch/powerpc

I couldnt find the start.S for e6500 power pc core .

Could you please suggest something?

Thanks.

0 件の賞賛
返信

2,658件の閲覧回数
ufedor
NXP Employee
NXP Employee

The same "start.S" is used for all processors of the "mpc85xx" branch including T2080.

0 件の賞賛
返信