SRK list in ISBC CSF header

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SRK list in ISBC CSF header

Jump to solution
1,602 Views
dmitri_lechtchinski
Contributor III

Hello,


If I use a list of public keys (by enabling "Srk table flag" in CSF header), and generate the appropriate SRKH value for programming in fuse, does this mean that every ISBC CSF header from now on must include the same list of all public keys and in the same order?
Is there an example for running uni_sign tool with such configuration? The document "QorIQ SDK v2.0-1703 Documentation" only includes examples for a single key.


Thank you,
Dmitri

 

Labels (1)
0 Kudos
Reply
1 Solution
1,575 Views
yipingwang
NXP TechSupport
NXP TechSupport

Yes, that means all your T2080 with the same SRKH value must use the same

list of all public keys. However, you can choose to use any one of the

maximum four keys. i.e. Since the SRKH is based on your keys, once the SRKH

is burned, you cannot add more keys to the list as it will alter the SRKH

value and make the checking fail.

 

In any of the input_files in the CST folder(e.g.

cst/input_files/uni_sign/t1_t2_t4/input_uboot_nor_secure) , you can:

#####

# USAGE (for 4080/5020/5040/3041/2041/1010/913x): PRI_KEY = <key1.pri>

# USAGE (for 1040/C290/9164/4240): PRI_KEY = <key1.pri>, <key2.pri>,

<key3.pri>, <key4.pri>

 

# PRI_KEY (Default private key :srk.pri) - [Optional]

PRI_KEY=srk1.pri, srk2.pri, srk3.pri, srk4.pri

# PUB_KEY (Default public key :srk.pub) - [Optional]

PUB_KEY=srk1.pub, srk2.pub, srk3.pub, srk4.pub,

# Please provide KEY_SELECT(between 1 to 4) (Required for

1040/C290/9164/4240 only) - [Optional]

KEY_SELECT=3

#####

In this case, it will use srk3.pri and srk3.pub to sign the image. If later

you revoke key #3, then the secure boot will fail with the image you sign by

srk3.pri/pub. You still can use key1,2, or 4 to sign image and run on your

T2080.

View solution in original post

1 Reply
1,576 Views
yipingwang
NXP TechSupport
NXP TechSupport

Yes, that means all your T2080 with the same SRKH value must use the same

list of all public keys. However, you can choose to use any one of the

maximum four keys. i.e. Since the SRKH is based on your keys, once the SRKH

is burned, you cannot add more keys to the list as it will alter the SRKH

value and make the checking fail.

 

In any of the input_files in the CST folder(e.g.

cst/input_files/uni_sign/t1_t2_t4/input_uboot_nor_secure) , you can:

#####

# USAGE (for 4080/5020/5040/3041/2041/1010/913x): PRI_KEY = <key1.pri>

# USAGE (for 1040/C290/9164/4240): PRI_KEY = <key1.pri>, <key2.pri>,

<key3.pri>, <key4.pri>

 

# PRI_KEY (Default private key :srk.pri) - [Optional]

PRI_KEY=srk1.pri, srk2.pri, srk3.pri, srk4.pri

# PUB_KEY (Default public key :srk.pub) - [Optional]

PUB_KEY=srk1.pub, srk2.pub, srk3.pub, srk4.pub,

# Please provide KEY_SELECT(between 1 to 4) (Required for

1040/C290/9164/4240 only) - [Optional]

KEY_SELECT=3

#####

In this case, it will use srk3.pri and srk3.pub to sign the image. If later

you revoke key #3, then the secure boot will fail with the image you sign by

srk3.pri/pub. You still can use key1,2, or 4 to sign image and run on your

T2080.