T2080 Basic boot code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T2080 Basic boot code

1,848 次查看
Faizanbaig
Contributor IV

Hi,

We are trying to initialize stack, CPU , RAM on T2080ARDB but we are not finding basic baremetal boot code for initialization.

Could you please help us with any pointers or reference to look into?

 

Thanks,

Faizanbaig Inamdar

标签 (1)
标记 (2)
0 项奖励
回复
3 回复数

1,842 次查看
ufedor
NXP Employee
NXP Employee

There are no such separate software components from NXP.

Available complex reference is U-Boot source code from the Linux SDK.

The SDK v2.0 can be downloaded from:

http://www.nxp.com/products/software-and-tools/run-time-software/linux-sdk/linux-sdk-for-qoriq-proce...

0 项奖励
回复

1,830 次查看
Faizanbaig
Contributor IV

Thanks for the response.

I installed SDK on linux and my need is to get start.S file for T2080rdb e6500 core.

I migrated to below path after sdk installation:

/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b/tmp/work/t2080rdb_64b-fsl-linux/u-boot-qoriq/2016.09+fslgit-r0/git/arch/powerpc

I couldnt find the start.S for e6500 power pc core .

Could you please suggest something?

Thanks.

0 项奖励
回复

1,826 次查看
ufedor
NXP Employee
NXP Employee

The same "start.S" is used for all processors of the "mpc85xx" branch including T2080.

0 项奖励
回复