T1042 Support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T1042 Support

2,687 次查看
sivakumar_t
Contributor I

I am planning to use T1042 QorIQ Processor for Control System applications.life of the part availability and the RTOS support.Whether Code warrior tool can be used for development without RTOS. Plese provide the Programming tool and the Debugging tool support for T1042 Processor.

标签 (1)
0 项奖励
回复
2 回复数

2,370 次查看
dave4763
Contributor I

please answer the end of life question. is it 5yrs, 10yrs, 15yrs, or more?

0 项奖励
回复

2,606 次查看
ufedor
NXP Employee
NXP Employee

CodeWarrior for Power Architecture is a universal IDE which contains:

  • Flash programmer
  • Hardware diagnostics
  • Linux application debug
  • Bare-Board multicore debug
  • Integrated GCC Build Tools/Project Management
  • CodeWarrior Build Tools
  • Trace (bare metal; selected cores only)

CodeWarrior® Development Suite for Networked Applications | NXP 

Required hardware components are:

CodeWarrior TAP (CWH-CTP-BASE-HE):
https://www.nxp.com/design/software/development-software/codewarrior-development-tools/run-control-d...

CWTAP Probe Tip for PowerQUICC II/III, QorIQ MPUs (CWH-CTP-COP-YE):

https://www.nxp.com/design/software/development-software/codewarrior-development-tools/run-control-d...

0 项奖励
回复