T1042 Support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1042 Support

2,733 Views
sivakumar_t
Contributor I

I am planning to use T1042 QorIQ Processor for Control System applications.life of the part availability and the RTOS support.Whether Code warrior tool can be used for development without RTOS. Plese provide the Programming tool and the Debugging tool support for T1042 Processor.

Labels (1)
0 Kudos
Reply
2 Replies

2,416 Views
dave4763
Contributor I

please answer the end of life question. is it 5yrs, 10yrs, 15yrs, or more?

0 Kudos
Reply

2,652 Views
ufedor
NXP Employee
NXP Employee

CodeWarrior for Power Architecture is a universal IDE which contains:

  • Flash programmer
  • Hardware diagnostics
  • Linux application debug
  • Bare-Board multicore debug
  • Integrated GCC Build Tools/Project Management
  • CodeWarrior Build Tools
  • Trace (bare metal; selected cores only)

CodeWarrior® Development Suite for Networked Applications | NXP 

Required hardware components are:

CodeWarrior TAP (CWH-CTP-BASE-HE):
https://www.nxp.com/design/software/development-software/codewarrior-development-tools/run-control-d...

CWTAP Probe Tip for PowerQUICC II/III, QorIQ MPUs (CWH-CTP-COP-YE):

https://www.nxp.com/design/software/development-software/codewarrior-development-tools/run-control-d...

0 Kudos
Reply