T1042 DDR4 ALERT Query

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1042 DDR4 ALERT Query

3,002件の閲覧回数
gokulkrishnan
Contributor III

Hello,

I am using a DDR4 x32 configuration with a single x8 ECC chip. There are 3 Alert signals from the DDR chips. There is only one MAPAR_ERR_B pin. So how should I connect it? Please advise. 

Regards 

Gokul

ラベル(1)
0 件の賞賛
返信
1 返信

2,770件の閲覧回数
ufedor
NXP Employee
NXP Employee

The DDR4 chip ALERT signal is open-drain, so all ALERT signals have to be connected together and pulled up to GVDD through 4.7-10 kOhm.

0 件の賞賛
返信