Is there an error in the QorIQ SDK 2.0 documentation?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there an error in the QorIQ SDK 2.0 documentation?

Jump to solution
1,408 Views
matthewrendell
Contributor I

Hello,

I am using QorIQ SDK 2.0 and there appears to be an error in QORIQSDK21611 Rev. 0 (QorIQ SDK v2.0-1611 Documentation) for the T1040D4RDB. In table 92 the 'Linux.uImage (alt bank)' location is defined as 0xEE020000, I'm pretty sure it's supposed to be 0xEC020000, can anyone confirm please?

Thanks,

Mat.

Labels (1)
Tags (2)
1 Solution
1,322 Views
ufedor
NXP Employee
NXP Employee

You are right.

The 0xEE020000 is a typo - should be 0xEC020000.

View solution in original post

1 Reply
1,323 Views
ufedor
NXP Employee
NXP Employee

You are right.

The 0xEE020000 is a typo - should be 0xEC020000.