T1042 DDR4 ALERT Query

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1042 DDR4 ALERT Query

3,017 Views
gokulkrishnan
Contributor III

Hello,

I am using a DDR4 x32 configuration with a single x8 ECC chip. There are 3 Alert signals from the DDR chips. There is only one MAPAR_ERR_B pin. So how should I connect it? Please advise. 

Regards 

Gokul

Labels (1)
0 Kudos
Reply
1 Reply

2,785 Views
ufedor
NXP Employee
NXP Employee

The DDR4 chip ALERT signal is open-drain, so all ALERT signals have to be connected together and pulled up to GVDD through 4.7-10 kOhm.

0 Kudos
Reply