Are there any gotchas associated with the single oscillator source mode described in the T1040RM Section 4.6.7.1.1? This looks like a good strategy if I only require one oscillator.
It is required to check that projected high speed interfaces configuration could be implemented using single oscillator source referring the QorIQ T1040 Reference Manual, Table 31-3. Valid SerDes Reference Clocks and RCW Encodings (SGMII-2.5G (3.125 Gbps)).