T1040 what are the tradeoffs for selecting "single oscillator source" vs "multiple reference clock mode"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1040 what are the tradeoffs for selecting "single oscillator source" vs "multiple reference clock mode"

503 Views
adamgarrison
Contributor III

Are there any gotchas associated with the single oscillator source mode described in the T1040RM Section 4.6.7.1.1?  This looks like a good strategy if I only require one oscillator.

Labels (1)
0 Kudos
1 Reply

433 Views
ufedor
NXP Employee
NXP Employee

It is required to check that projected high speed interfaces configuration could be implemented using single oscillator source referring the QorIQ T1040 Reference Manual, Table 31-3. Valid SerDes Reference Clocks and RCW Encodings (SGMII-2.5G (3.125 Gbps)).

0 Kudos