T1040 what are the tradeoffs for selecting "single oscillator source" vs "multiple reference clock mode"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T1040 what are the tradeoffs for selecting "single oscillator source" vs "multiple reference clock mode"

504 次查看
adamgarrison
Contributor III

Are there any gotchas associated with the single oscillator source mode described in the T1040RM Section 4.6.7.1.1?  This looks like a good strategy if I only require one oscillator.

标签 (1)
0 项奖励
1 回复

434 次查看
ufedor
NXP Employee
NXP Employee

It is required to check that projected high speed interfaces configuration could be implemented using single oscillator source referring the QorIQ T1040 Reference Manual, Table 31-3. Valid SerDes Reference Clocks and RCW Encodings (SGMII-2.5G (3.125 Gbps)).

0 项奖励