Reset vector address and loading u-boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reset vector address and loading u-boot

Jump to solution
1,105 Views
noufalp90
Contributor III

Hi all,

We are working on a custom board with T2081 SOC. I am new to the Tseries chip and when I go through the RM, I came across following section, "Boot Space Translation" where it is mentioned that 

```

When each core comes out of reset, its MMU has one 4 KB page defined at
0x0_FFFF_Fnnn. Each core begins execution with the instruction at effective address
0x0_FFFF_FFFC. To get this instruction, the core's first instruction fetch is a burst read
of boot code from effective address 0x0_FFFF_FFC0

```

 

So my question is, If I flash u-boot binary in NOR flash, how the core knows about the exact address of NOR flash to load u-boot image from NOR flash address and load to DDR.

Is there any register or configuration which instructs PC to jump to u-boot vector address and starts loading u-boot from NOR address when core begins execution at 0x0_FFFF_FFFC?

T2080RDB T2080 

Thanks,

Noufal P

0 Kudos
Reply
1 Solution
1,047 Views
yipingwang
NXP TechSupport
NXP TechSupport

For boot from NOR flash, the system always fetches the first instruction from the end of NOR flash.

You need to build u-boot image to configure reset vector at the end of NOR flash. For example:

#ifndef CONFIG_RESET_VECTOR_ADDRESS
#define CONFIG_RESET_VECTOR_ADDRESS 0xeffffffc
#endif

#define CONFIG_SYS_FLASH_BASE 0xe8000000

View solution in original post

1 Reply
1,048 Views
yipingwang
NXP TechSupport
NXP TechSupport

For boot from NOR flash, the system always fetches the first instruction from the end of NOR flash.

You need to build u-boot image to configure reset vector at the end of NOR flash. For example:

#ifndef CONFIG_RESET_VECTOR_ADDRESS
#define CONFIG_RESET_VECTOR_ADDRESS 0xeffffffc
#endif

#define CONFIG_SYS_FLASH_BASE 0xe8000000