Initialize RAM alone in u-boot at T4160

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Initialize RAM alone in u-boot at T4160

Jump to solution
2,101 Views
vinothkumars
Senior Contributor IV

Hi,

I am using T4160QDS machine as a target, CodeWarrior Flashprogrammer for flash and lauterbach trace32 debugger for emulating purpose.

By using these tools I want to initialize DDR alone.  

Thanks & Regards,

VinothS

Regards,
Vinothkumar Sekar
Labels (1)
0 Kudos
Reply
1 Solution
2,016 Views
alexander_yakov
NXP Employee
NXP Employee

Please look our target initialization file, supplied with CodeWarrior, and use as reference.

[your CodeWarrior installation folder] \PA\PA_Support\Initialization_Files\QorIQ_T4\T4160QDS_init_core.tcl


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,017 Views
alexander_yakov
NXP Employee
NXP Employee

Please look our target initialization file, supplied with CodeWarrior, and use as reference.

[your CodeWarrior installation folder] \PA\PA_Support\Initialization_Files\QorIQ_T4\T4160QDS_init_core.tcl


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply