Initialize RAM alone in u-boot at T4160

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Initialize RAM alone in u-boot at T4160

跳至解决方案
2,098 次查看
vinothkumars
Senior Contributor IV

Hi,

I am using T4160QDS machine as a target, CodeWarrior Flashprogrammer for flash and lauterbach trace32 debugger for emulating purpose.

By using these tools I want to initialize DDR alone.  

Thanks & Regards,

VinothS

Regards,
Vinothkumar Sekar
标签 (1)
0 项奖励
回复
1 解答
2,013 次查看
alexander_yakov
NXP Employee
NXP Employee

Please look our target initialization file, supplied with CodeWarrior, and use as reference.

[your CodeWarrior installation folder] \PA\PA_Support\Initialization_Files\QorIQ_T4\T4160QDS_init_core.tcl


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,014 次查看
alexander_yakov
NXP Employee
NXP Employee

Please look our target initialization file, supplied with CodeWarrior, and use as reference.

[your CodeWarrior installation folder] \PA\PA_Support\Initialization_Files\QorIQ_T4\T4160QDS_init_core.tcl


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复