Initialize RAM alone in u-boot at T4160

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Initialize RAM alone in u-boot at T4160

ソリューションへジャンプ
2,054件の閲覧回数
vinothkumars
Senior Contributor IV

Hi,

I am using T4160QDS machine as a target, CodeWarrior Flashprogrammer for flash and lauterbach trace32 debugger for emulating purpose.

By using these tools I want to initialize DDR alone.  

Thanks & Regards,

VinothS

Regards,
Vinothkumar Sekar
ラベル(1)
0 件の賞賛
返信
1 解決策
1,969件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Please look our target initialization file, supplied with CodeWarrior, and use as reference.

[your CodeWarrior installation folder] \PA\PA_Support\Initialization_Files\QorIQ_T4\T4160QDS_init_core.tcl


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,970件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Please look our target initialization file, supplied with CodeWarrior, and use as reference.

[your CodeWarrior installation folder] \PA\PA_Support\Initialization_Files\QorIQ_T4\T4160QDS_init_core.tcl


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信