How to configure b4860qds to automatically reboot when power-cycled

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to configure b4860qds to automatically reboot when power-cycled

1,176 次查看
victorgomez
Contributor II

Hi!

I connected my b4860qds board to a power-server, but it is not working by default as expected. When I reboot the board from the power server (power-cycle), the board just shuts down, it doesnt reboot. Is there any pin or anything in the board Ineed to change to make it possible to power-cycle remotely?

Thanks!

标记 (3)
0 项奖励
回复
1 回复

1,104 次查看
ufedor
NXP Employee
NXP Employee

You wrote:

> When I reboot the board from the power server (power-cycle),

> the board just shuts down, it doesnt reboot.

Please check whether installing J11 jumper solves the isue.

If no, it is needed to determine what is the difference between local power-cycle and remote.

May be remote control signal is too short?

How exacly the remote power-cycle is implemented?

0 项奖励
回复