DEBUG OF T1042

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DEBUG OF T1042

1,498件の閲覧回数
gokulkrishnan
Contributor III

Hi,

I was using the T1042 processor for my design. For the debug of the board is there any debug header we need to add other than the Jtag header we will have.

Regards 

Gokul

ラベル(1)
1 返信

1,379件の閲覧回数
ufedor
NXP Employee
NXP Employee

The request is not fully clear.

To debug PowePC processors by the CodeWarrior the following hardware components are needed:

CodeWarrior® TAP:

CodeWarrior TAP|NXP 

Power ArchPitecture® processor ( COP ) Probe Tips for CodeWarrior® TAP:

Power Architecture processor for CodeWarrior|NXP 

0 件の賞賛
返信