DEBUG OF T1042

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DEBUG OF T1042

1,499 Views
gokulkrishnan
Contributor III

Hi,

I was using the T1042 processor for my design. For the debug of the board is there any debug header we need to add other than the Jtag header we will have.

Regards 

Gokul

Labels (1)
1 Reply

1,380 Views
ufedor
NXP Employee
NXP Employee

The request is not fully clear.

To debug PowePC processors by the CodeWarrior the following hardware components are needed:

CodeWarrior® TAP:

CodeWarrior TAP|NXP 

Power ArchPitecture® processor ( COP ) Probe Tips for CodeWarrior® TAP:

Power Architecture processor for CodeWarrior|NXP 

0 Kudos
Reply