DDR3 Power Connection on T1024RDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR3 Power Connection on T1024RDB

ソリューションへジャンプ
1,930件の閲覧回数
bltuna
Contributor II

Hi,

Below is the power connection of the DDR3 that is presented on the T1024RDB schematic. I couldn't understand why such a connection (highlighted portion) is made.

ddr3.PNG

ラベル(1)
タグ(3)
1 解決策
1,793件の閲覧回数
r8070z
NXP Employee
NXP Employee

pastedImage_1.png

This figure is from T1040QDS schematics where they explains that connection. For the T1024RDB schematics it should sounds like “Decoupling between 1V35_SLP and 1V35 power split located under DIMM. Place these caps around DDR Power Pin areas to stitch return current flow for Address and command signals.”

元の投稿で解決策を見る

1 返信
1,794件の閲覧回数
r8070z
NXP Employee
NXP Employee

pastedImage_1.png

This figure is from T1040QDS schematics where they explains that connection. For the T1024RDB schematics it should sounds like “Decoupling between 1V35_SLP and 1V35 power split located under DIMM. Place these caps around DDR Power Pin areas to stitch return current flow for Address and command signals.”