DDR3 Power Connection on T1024RDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR3 Power Connection on T1024RDB

Jump to solution
1,280 Views
bltuna
Contributor II

Hi,

Below is the power connection of the DDR3 that is presented on the T1024RDB schematic. I couldn't understand why such a connection (highlighted portion) is made.

ddr3.PNG

Labels (1)
Tags (3)
1 Solution
1,143 Views
r8070z
NXP Employee
NXP Employee

pastedImage_1.png

This figure is from T1040QDS schematics where they explains that connection. For the T1024RDB schematics it should sounds like “Decoupling between 1V35_SLP and 1V35 power split located under DIMM. Place these caps around DDR Power Pin areas to stitch return current flow for Address and command signals.”

View solution in original post

1 Reply
1,144 Views
r8070z
NXP Employee
NXP Employee

pastedImage_1.png

This figure is from T1040QDS schematics where they explains that connection. For the T1024RDB schematics it should sounds like “Decoupling between 1V35_SLP and 1V35 power split located under DIMM. Place these caps around DDR Power Pin areas to stitch return current flow for Address and command signals.”