DDR Value update to T4160 system

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

DDR Value update to T4160 system

跳至解决方案
2,371 次查看
vinothkumars
Senior Contributor IV

Hi All,

I am using T4160QDS-64b Machine. SDK Version is 2.0 and download SDK (QorIQ Linux SDK v2.0 SOURCE.iso ) from  the following link, 

https://nxp.flexnetoperations.com/control/frse/download?element=7726177

 

U-boot image also built successfully. Finally, I done the DDR Calibration using Codewarrior IDE.

Now, I struggle in update ddr values in T4160QDS-64b U-boot Source Code.

Please find the attachment of U-boot Source (t4qds) and DDR Values(T4160_v2_0_codewarrior_regs.regs) from Codewarrior IDE for T4160QDS-64b.

How will update DDR Value in U-boot Source to T4160QDS-64b Machine ?

Thank you so much in advance for all your help! 

Thanks & Regards,

Vinoths

Regards,
Vinothkumar Sekar
标签 (1)
0 项奖励
回复
1 解答
2,207 次查看
Pavel
NXP Employee
NXP Employee

See the AN5279 about using QCVS for u-boot DDR configuration:

https://www.nxp.com/docs/en/application-note/AN5279.pdf

Have a great day,
Pavel Chubakov

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,208 次查看
Pavel
NXP Employee
NXP Employee

See the AN5279 about using QCVS for u-boot DDR configuration:

https://www.nxp.com/docs/en/application-note/AN5279.pdf

Have a great day,
Pavel Chubakov

0 项奖励
回复
2,207 次查看
vinothkumars
Senior Contributor IV

Hi Pavel,

Thank you for your reply.  

Thanks & Regards,

VinothS

Regards,
Vinothkumar Sekar
0 项奖励
回复