DDR Value update to T4160 system

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR Value update to T4160 system

ソリューションへジャンプ
2,374件の閲覧回数
vinothkumars
Senior Contributor IV

Hi All,

I am using T4160QDS-64b Machine. SDK Version is 2.0 and download SDK (QorIQ Linux SDK v2.0 SOURCE.iso ) from  the following link, 

https://nxp.flexnetoperations.com/control/frse/download?element=7726177

 

U-boot image also built successfully. Finally, I done the DDR Calibration using Codewarrior IDE.

Now, I struggle in update ddr values in T4160QDS-64b U-boot Source Code.

Please find the attachment of U-boot Source (t4qds) and DDR Values(T4160_v2_0_codewarrior_regs.regs) from Codewarrior IDE for T4160QDS-64b.

How will update DDR Value in U-boot Source to T4160QDS-64b Machine ?

Thank you so much in advance for all your help! 

Thanks & Regards,

Vinoths

Regards,
Vinothkumar Sekar
ラベル(1)
0 件の賞賛
返信
1 解決策
2,210件の閲覧回数
Pavel
NXP Employee
NXP Employee

See the AN5279 about using QCVS for u-boot DDR configuration:

https://www.nxp.com/docs/en/application-note/AN5279.pdf

Have a great day,
Pavel Chubakov

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,211件の閲覧回数
Pavel
NXP Employee
NXP Employee

See the AN5279 about using QCVS for u-boot DDR configuration:

https://www.nxp.com/docs/en/application-note/AN5279.pdf

Have a great day,
Pavel Chubakov

0 件の賞賛
返信
2,210件の閲覧回数
vinothkumars
Senior Contributor IV

Hi Pavel,

Thank you for your reply.  

Thanks & Regards,

VinothS

Regards,
Vinothkumar Sekar
0 件の賞賛
返信