Problem: der MQX CW MCU v10.5 erkennt den Lizensierungsfile nicht !!!!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Problem: der MQX CW MCU v10.5 erkennt den Lizensierungsfile nicht !!!!

跳至解决方案
954 次查看
projektecarus
Contributor II

Problem: der MQX CW MCU v10.5 erkennt den Lizensierungsfile nicht !!!!

标签 (1)
0 项奖励
回复
1 解答
823 次查看
TICS_Fiona
NXP Employee
NXP Employee

Where did you save the license file? Please place it under \MCU subfolder.

Are you logging on Windows as Administrator, and whether the system time was set on a past date?

In addition, for some products (e.g. Coldfire),  only the Professional Edition supports the Kernel-aware Debug for MQX.

For the difference of each Edition, please view the webpage below:

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_SUITES&tid=CWH

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
823 次查看
trytohelp
NXP Employee
NXP Employee

Hallo,

In addition to Fiona ...

Do you have a license issue ?

By default the installation includes an evaluation license file.

This evaluation license is based on the Professional Suite license.

You're using CW for MCU V10.5.

CW for MCU V10.6.4 is the last version and a new patch MCU v10.6.5 has been released 1 month ago.

Depending of your application it could be interesting to move to the last version.

You can access it via the Freescale Web site.

If you purchased a registration, the license for MCU V10.5 is valid for MCU V10.6 too.

What's about MQX ?

MQX must be installed separately and don't require license file.

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
824 次查看
TICS_Fiona
NXP Employee
NXP Employee

Where did you save the license file? Please place it under \MCU subfolder.

Are you logging on Windows as Administrator, and whether the system time was set on a past date?

In addition, for some products (e.g. Coldfire),  only the Professional Edition supports the Kernel-aware Debug for MQX.

For the difference of each Edition, please view the webpage below:

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_SUITES&tid=CWH

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复