License Generation Issue : Freescale Codewarrior professional edition

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

License Generation Issue : Freescale Codewarrior professional edition

跳至解决方案
5,147 次查看
rubykrishna
Contributor III


Hi All,

 

We recently bought 3 floating license for Codewarrior professional edition which comes under three different entitlement ID's. I  encountered few issues

 

1. When i registered the professional edition with freescale login ( for generating the license file),  Drop-down list shows that i can download multiple IDE's from freescale(refer attachement 1) .  When i tried to download the license file it shows the following error. Does codewarrior professional edition supports only codewarrior IDE?? ( Refer attachement 2). Will it wont support other IDE's like powerpc architecture, star Code DSP,MPC's?

 

2. 3 Floating license may generate three different license file. Is it possible to merge all three license file into a single license file??

   
 

 


标签 (1)
1 解答
4,554 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi ruby,

yes you merge all those license.dat files into one. it can support all the series.


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
4 回复数
4,554 次查看
rubykrishna
Contributor III

Hi Zhang,

Thanks for reverting back. We procured floating license Codewarrior professional edition(generic). License.dat which we tend to generate shall support all Codewarrior IDe's right? In our team one may  need 10.6(s12z family) whereas i need  5.1(s12xFAMILY) someone may use MPC555x series!.... To put it simple we need to generate the license file which support all Codewarrior IDE's.

Please help me on this regard!!

0 项奖励
回复
4,555 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi ruby,

yes you merge all those license.dat files into one. it can support all the series.


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
4,554 次查看
rubykrishna
Contributor III

Hi Zhang,

Its working. Im able to compile the code > 32KB size. How could i ensure its a professional edition?? I didnt find any difference in the codewarrrior GUI!!

0 项奖励
回复
4,554 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

hi ruby,

different architecture needs different CW IDE version support. HCS12 MCU is supported by CW for HCS12(x), starcore is supported by CW for startcore DSP, etc.  each CW IDE use each license. for example, the CW for HCS12 license can only for for CW for HCS12(x). it can't work for other CW IDE.

regarding to your second question, yes, you can merge several licenses to one license.dat file. see this thread:

https://community.freescale.com/thread/340841

can this help?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------