Is it possible to access floating licence through VPN?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to access floating licence through VPN?

ソリューションへジャンプ
2,344件の閲覧回数
francisthiffaul
Contributor I

Hi, I'm using software Freescale CodeWarrior 7.1 with a floating licence installed on a local licence server. I need to emulate my code at customer office... So, there is it a way to access this floating licence from my customer office through VPN? We tried it and it doesn't seem to work, there is it a particular setting that should be done?

Thanks in advance for your support,

Francis

0 件の賞賛
返信
1 解決策
2,050件の閲覧回数
TomasPaez
NXP Employee
NXP Employee

Yes it is possible as long as you have access to server.

if there is any TCP/IP port closed make sure 27000-27009 range is open since these are the default range used. 

You can also specify this on the license file

SERVER servname 00145MACETHC9A [portnumber]
USE_SERVER
DAEMON metrowks

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,051件の閲覧回数
TomasPaez
NXP Employee
NXP Employee

Yes it is possible as long as you have access to server.

if there is any TCP/IP port closed make sure 27000-27009 range is open since these are the default range used. 

You can also specify this on the license file

SERVER servname 00145MACETHC9A [portnumber]
USE_SERVER
DAEMON metrowks

0 件の賞賛
返信