Is it possible to access floating licence through VPN?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is it possible to access floating licence through VPN?

跳至解决方案
2,350 次查看
francisthiffaul
Contributor I

Hi, I'm using software Freescale CodeWarrior 7.1 with a floating licence installed on a local licence server. I need to emulate my code at customer office... So, there is it a way to access this floating licence from my customer office through VPN? We tried it and it doesn't seem to work, there is it a particular setting that should be done?

Thanks in advance for your support,

Francis

0 项奖励
回复
1 解答
2,056 次查看
TomasPaez
NXP Employee
NXP Employee

Yes it is possible as long as you have access to server.

if there is any TCP/IP port closed make sure 27000-27009 range is open since these are the default range used. 

You can also specify this on the license file

SERVER servname 00145MACETHC9A [portnumber]
USE_SERVER
DAEMON metrowks

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,057 次查看
TomasPaez
NXP Employee
NXP Employee

Yes it is possible as long as you have access to server.

if there is any TCP/IP port closed make sure 27000-27009 range is open since these are the default range used. 

You can also specify this on the license file

SERVER servname 00145MACETHC9A [portnumber]
USE_SERVER
DAEMON metrowks

0 项奖励
回复