Codewarrior 5.2 sometimes falls back to trial license

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Codewarrior 5.2 sometimes falls back to trial license

跳至解决方案
1,821 次查看
adrianteuscher
Contributor I

Hi,

We have a network (floating) license for Codewarrior Classic 5.2. After a few build's of my software, the linker error "L4025: This limited version allows only 65536 bytes of C code" appears and the link failed. When i wait a minute or two, and build again, it works as exprected.

We also use Codewarrior 10.6 with the same license model - without problems.

 

Thank you in advance!

Adrian

标签 (1)
0 项奖励
回复
1 解答
1,641 次查看
TomasPaez
NXP Employee
NXP Employee

It will be good to see the log file located in LMTools.exe utility , also wondering if you are using comm

Check the log file on the path specified

   pastedImage_0.png

If you are using multiple clients, sometime check in does not occur right away this might be a root cause.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,642 次查看
TomasPaez
NXP Employee
NXP Employee

It will be good to see the log file located in LMTools.exe utility , also wondering if you are using comm

Check the log file on the path specified

   pastedImage_0.png

If you are using multiple clients, sometime check in does not occur right away this might be a root cause.

0 项奖励
回复