Codewarrior 5.2 sometimes falls back to trial license

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior 5.2 sometimes falls back to trial license

Jump to solution
1,792 Views
adrianteuscher
Contributor I

Hi,

We have a network (floating) license for Codewarrior Classic 5.2. After a few build's of my software, the linker error "L4025: This limited version allows only 65536 bytes of C code" appears and the link failed. When i wait a minute or two, and build again, it works as exprected.

We also use Codewarrior 10.6 with the same license model - without problems.

 

Thank you in advance!

Adrian

Labels (1)
0 Kudos
Reply
1 Solution
1,612 Views
TomasPaez
NXP Employee
NXP Employee

It will be good to see the log file located in LMTools.exe utility , also wondering if you are using comm

Check the log file on the path specified

   pastedImage_0.png

If you are using multiple clients, sometime check in does not occur right away this might be a root cause.

View solution in original post

0 Kudos
Reply
1 Reply
1,613 Views
TomasPaez
NXP Employee
NXP Employee

It will be good to see the log file located in LMTools.exe utility , also wondering if you are using comm

Check the log file on the path specified

   pastedImage_0.png

If you are using multiple clients, sometime check in does not occur right away this might be a root cause.

0 Kudos
Reply