Codewarrior 5.2 sometimes falls back to trial license

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior 5.2 sometimes falls back to trial license

ソリューションへジャンプ
1,820件の閲覧回数
adrianteuscher
Contributor I

Hi,

We have a network (floating) license for Codewarrior Classic 5.2. After a few build's of my software, the linker error "L4025: This limited version allows only 65536 bytes of C code" appears and the link failed. When i wait a minute or two, and build again, it works as exprected.

We also use Codewarrior 10.6 with the same license model - without problems.

 

Thank you in advance!

Adrian

ラベル(1)
0 件の賞賛
返信
1 解決策
1,640件の閲覧回数
TomasPaez
NXP Employee
NXP Employee

It will be good to see the log file located in LMTools.exe utility , also wondering if you are using comm

Check the log file on the path specified

   pastedImage_0.png

If you are using multiple clients, sometime check in does not occur right away this might be a root cause.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,641件の閲覧回数
TomasPaez
NXP Employee
NXP Employee

It will be good to see the log file located in LMTools.exe utility , also wondering if you are using comm

Check the log file on the path specified

   pastedImage_0.png

If you are using multiple clients, sometime check in does not occur right away this might be a root cause.

0 件の賞賛
返信