Code Warrior license

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code Warrior license

1,926件の閲覧回数
fabiofontana
Contributor I

Hi,

We bought the license for the CodeWarrior Specialist Tool Pack - Node locked version with the p/n CWA-LS-SPLST-NL, plus the USB Dongle CWH-DONGLE.

I made the license registration as per disk serial number instead of FLEX-ID, in order to use the usb-dongle. How can I roll-back the licence in order to make a right FLEX-ID registration?

Registered data is 01/12/2016 and registered to Fabio Fontana.

Thanks.

Fabio.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,497件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Fabio,

You've generated the license file under DiskID and you want to lock it on USBDongleID.

You need to return the license and re-generate the license file.

    Licensing and Registration FAQ|NXP

There are some others docs on community:

    How to rehost CodeWarrior suite license

    Cannot Re-host a license - License Lists is empty (valid to generate a license file associated to a ...

Hope this will help


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信