CW licenses re-host problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CW licenses re-host problem

跳至解决方案
1,882 次查看
matteomantica
Contributor I

Dear All,

 

I need to re-host my CW perpetual floating licences to a new server. I cannot do it myself because I cannot see my licenses in the relative page. See the following screen:

127913_127913.jpgLicenseList.jpg

I the Order History page everything is correct and my orders are presents (see following screen)

127914_127914.jpgOrderHistory.jpg

How can I proceed?

 

Best Regards

Matteo

标签 (1)
0 项奖励
回复
1 解答
1,749 次查看
trytohelp
NXP Employee
NXP Employee

Hi Matteo,

You need to select the registration number via the Order History.

Then you can display all license file associated to a registration.

You can refer to the FAQs:

     Licensing and Registration FAQ|NXP

Else there are some info on community:

     How to rehost CodeWarrior suite license

     Cannot Re-host a license - License Lists is empty (valid to generate a license file associated to a...   

Now if you're using a classic tool, you could have some problem after rehost.

In this case, to avoid problem we can re-encrypt the license.

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,750 次查看
trytohelp
NXP Employee
NXP Employee

Hi Matteo,

You need to select the registration number via the Order History.

Then you can display all license file associated to a registration.

You can refer to the FAQs:

     Licensing and Registration FAQ|NXP

Else there are some info on community:

     How to rehost CodeWarrior suite license

     Cannot Re-host a license - License Lists is empty (valid to generate a license file associated to a...   

Now if you're using a classic tool, you could have some problem after rehost.

In this case, to avoid problem we can re-encrypt the license.

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复