mc33771C open line (cell terminal open detect)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

mc33771C open line (cell terminal open detect)

跳至解决方案
1,569 次查看
Wan
Contributor III

Hi ,NXP Enginess and All

I encountered some problems during the development of MC33771C sampling line open detection.

1th:Stop the cyclemeasure the cell voltage;

2th: Go to the diag mode,configer the sys_cfg2[go2diag] =1,

3th:  Control the switch of ODD or EVEN  sysdiag[CT_OL_ODD] =1 or sysdiag[CT_OL_EVEN] =1,

4th: Init the ADC_config;

5th :read the cell voltage;

I cut the line cell_11  measure the cell voltage by up way。cut lines voltage is more than normal‘s cells voltage , i think the cut lines volteage close zero.

Wan_0-1703148932058.png

where the switchs cotrol, register sys_diag[CT_OL_ODD/CT_OL_EVEN/CB_OL_ODD/CB_OL_EVEN]?

Wan_1-1703149520190.png

 In the end , i hope you can help me slove the problems!

thanks sir!

0 项奖励
回复
1 解答
1,526 次查看
guoweisun
NXP TechSupport
NXP TechSupport

For this CTx Open Detect and Open Detect Functional Verification, please download the safety manual page 24 SM02,there is detail CONFIGURATION instructions:

guoweisun_0-1703490497871.png

 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,481 次查看
Wan
Contributor III
thanks guoweisun! 
 
I got the 《afety manual》 and achieved the open Detect.
0 项奖励
回复
1,554 次查看
Wan
Contributor III

Hello NXP Enginess and All:

     I checked the status by reading the register, I read the Sys_cfg1=0x1C41 and SYS_CFG1[GO2DIAG] =1 register to confirm that I into the diag statue and turn off the balace Sys_cfg1[MANUE_CB] =0, and found that I wrote Sys_diag[Ct_obb]=1 but read it as 0. I can't turn on an odd or even switch.

标记 (1)
0 项奖励
回复
1,527 次查看
guoweisun
NXP TechSupport
NXP TechSupport

For this CTx Open Detect and Open Detect Functional Verification, please download the safety manual page 24 SM02,there is detail CONFIGURATION instructions:

guoweisun_0-1703490497871.png

 

0 项奖励
回复