mc33771C open line (cell terminal open detect)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mc33771C open line (cell terminal open detect)

Jump to solution
1,571 Views
Wan
Contributor III

Hi ,NXP Enginess and All

I encountered some problems during the development of MC33771C sampling line open detection.

1th:Stop the cyclemeasure the cell voltage;

2th: Go to the diag mode,configer the sys_cfg2[go2diag] =1,

3th:  Control the switch of ODD or EVEN  sysdiag[CT_OL_ODD] =1 or sysdiag[CT_OL_EVEN] =1,

4th: Init the ADC_config;

5th :read the cell voltage;

I cut the line cell_11  measure the cell voltage by up way。cut lines voltage is more than normal‘s cells voltage , i think the cut lines volteage close zero.

Wan_0-1703148932058.png

where the switchs cotrol, register sys_diag[CT_OL_ODD/CT_OL_EVEN/CB_OL_ODD/CB_OL_EVEN]?

Wan_1-1703149520190.png

 In the end , i hope you can help me slove the problems!

thanks sir!

0 Kudos
Reply
1 Solution
1,528 Views
guoweisun
NXP TechSupport
NXP TechSupport

For this CTx Open Detect and Open Detect Functional Verification, please download the safety manual page 24 SM02,there is detail CONFIGURATION instructions:

guoweisun_0-1703490497871.png

 

View solution in original post

0 Kudos
Reply
3 Replies
1,483 Views
Wan
Contributor III
thanks guoweisun! 
 
I got the 《afety manual》 and achieved the open Detect.
0 Kudos
Reply
1,556 Views
Wan
Contributor III

Hello NXP Enginess and All:

     I checked the status by reading the register, I read the Sys_cfg1=0x1C41 and SYS_CFG1[GO2DIAG] =1 register to confirm that I into the diag statue and turn off the balace Sys_cfg1[MANUE_CB] =0, and found that I wrote Sys_diag[Ct_obb]=1 but read it as 0. I can't turn on an odd or even switch.

Tags (1)
0 Kudos
Reply
1,529 Views
guoweisun
NXP TechSupport
NXP TechSupport

For this CTx Open Detect and Open Detect Functional Verification, please download the safety manual page 24 SM02,there is detail CONFIGURATION instructions:

guoweisun_0-1703490497871.png

 

0 Kudos
Reply